FAQ

Q1

What are the High-speed Hand Dryer's advantages over warm air-type hand dryers?

A1

From the user standpoint, the biggest advantage is faster drying time. Compared with the 30 to 40 seconds required by warm-air dryers, the High-speed Hand Dryer reduces the time to 3-6 seconds.

Back
Q2

How is the drying time reduced?

A2

Unlike warm-air dryers, where the hands are dried while being rubbed together, the High-speed Hand Dryer utilizes nozzles on the inner sides of the unit where the hands are inserted. As the jets of air are directed at the hands, drops of water are literally forced off.

Back
Q3

How much wind is generated?

A3

Set to the "Hyper" position, the High-speed Hand Dryer generates roughly 3.6 cubic meters of wind per minute.

Back
Q4

Isn't it noisy?

A4

The High-speed Hand Dryer, set to the "Hyper" position, produces approximately 59dB of noise, or quieter than existing hand dryers. Since warm-air dryers operate considerably longer (30-40 seconds) than the 3-6 seconds needed for the High-speed Hand Dryer, overall noise exposure is dramatically reduced.

Back
Q5

Isn't the High-speed Hand Dryer more expensive than other types?

A5

Some conventional dryers are available for less than a thousand dollars (US). However, many users are dissatisfied with their longer, 30-40 second drying time, and some refrain from using them altogether. The High-speed Hand Dryer, even at a higher price, is certain to eliminate these type of user complaints. Used over an extended period, it will also be more economical than use of paper towels or cloth towels on rollers.

Back
Q6

Is the height adjustable?

A3

Once installed, the unit's height cannot be adjusted. The optimum position (for use by men or women) should be considered at the time of installation. The general installation guideline in Japan is a height of 89cm for men, 87cm for women.

Back
Q7

What is the usable life of the unit?

A7

Product life is determined by motor operation. A DC brushless motor gives the High-speed Hand Dryer a life expectancy of approximately seven years at 1000 uses daily. In areas that utilize high voltage power supply, the drying duration is extended very slightly, which may result in a slight reduction in product life.

Back
Q8

Can the High-speed Hand Dryer be used in locales with high temperature?

A8

The High-speed Hand Dryer design presumes use at ordinary room temperatures. If the unit is to be utilized at a location with higher than normal temperatures, it is advised that the necessary wiring precautions be taken. In general, the unit should not be used in any area where the temperature exceeds 40 degrees Celsius (104 degrees Fahrenheit).

Back
Q9

How about use in locales with high humidity?

A9

As long as conditions do not result in condensation ("dew") forming on the unit's internal parts, no problems are anticipated.

Back
Q10

Can the High-speed Hand Dryer be used in factories?

A10

The unit should not be utilized when chemical substances are on the hands. To disinfect, masking solutions can be applied, but cresylic acid (solutio cresoli saponata) cannot be utilized.

Back
Q11

What do first-time users need to know?

A11

The High-speed Hand Dryer is provided with explanatory stickers that provide simple instructions for first-time users.

Back
Q12

Is there any potential harm from keeping the hands inside the unit longer than necessary?

A12

To prevent potential abuse or misuse, the High-speed Hand Dryer incorporates a built-in timer that automatically halts operation after 30 seconds. Once the hands are removed, the unit resets and resumes normal operation.

Back
Q13

If a child were to hang by his hands from the unit, could it possibly be torn from its mountings and fall off the wall?

A13

If a model such as the JT-SB216ESH, for example, is securely fastened to the wall using the six mounting screws provided, it should be able to support a considerable load. However, such abuse should be avoided whenever possible. (Naturally, this presumes the wall itself is robust.)

Back
Q14

Can the unit be plugged into a conventional AC wall outlet?

A14

No, the unit requires direct wiring.

Back
Q15

Is extra wall reinforcement required when installing?

A15

We advise that the mounting plate be reinforced with a panel on the reverse side of the wall. In the case of mounting on concrete walls, metal wood screw plugs are advisable.

Back
High-speed Hand Dryer