FAQ

Q1

What are the High-speed Hand Dryer's advantages over warm-air dryers?

Q2

How is the drying time reduced?

Q3

How much wind is generated?

Q4

Isn't it noisy?

Q5

Isn't the High-speed Hand Dryer more expensive than other types?

Q6

Is the height adjustable?

Q7

What is the usable life of the unit?

Q8

Can the High-speed Hand Dryer be used in locales with high temperature?

Q9

How about use in locales with high humidity?

Q10

Can the High-speed Hand Dryer be used in factories?

Q11

What do first-time users need to know?

Q12

Is there any potential harm from keeping the hands inside the unit longer than necessary?

Q13

If a child were to hang by his hands from the unit, could it possibly be torn from its mountings and fall off the wall?

Q14

Can the unit be plugged into a conventional AC wall outlet?

Q15

Is extra wall reinforcement required when installing?

High-speed Hand Dryer