Installation

Hotel / Shop

Nordstrom U.S.A.

Restroom now provide a positive message to our clientele. Customer feedback is extremely positive.

"Our customers have clearly shown a preference for environmentally responsible options in the restrooms. Our new restrooms are low-water use, low-energy use, and now paper towel free. Before we used the Jet Towel, we avoided hand dryers because of the sound, slipping hazard, and most importantly the frustration caused by the older style of hand dryers. The Jet Towel is now a featured fixture in our restrooms."



Factors behind the decision to use the High-speed Hand Dryer:


1. Nordstrom needed a very quiet hand dryer to maintain pleasant atmosphere in the restrooms.
2. Low energy consumption was a major factor in deciding to use the Jet Towel.


Background to Installation Upgrading restrooms to become more eco-friendly
Previous drying system Paper towels
Installation sites Customer restrooms
throughout facility
Mandarin CANADA

Eye appeal is amazing, and our customers enjoy using this state-of-the-art hand drying.

"All of our restrooms are equipped with hand dryers and paper towels. We decided to try this hand dryer in our new restaurants. Overall, the customer feedback has been very good-they have been impressed with this modern approach and we have also reduced the use of paper towels."



Factors behind the decision to use the High-speed Hand Dryer:


1. It is so fast, and warm air blows immediately, there was a holding tray to collect excess water as well. So clever! No mess.

Background to Installation New builiding / Renovated building
Previous drying system Paper towels /
Conventional hand dryer
Installation sites Customer restrooms
throughout facility
Number installed 88 units
Marina Mandarin SHINGAPORE

We have greatly reduced our maintenance cost with Jet Towel as there's no need for us to replenish paper towels and remove the waste.

"The installation of the Jet Towels in our restrooms helps reduce cleaning and operation costs significantly. It also reduces paper waste and offers rapid drying for our guests. There is less cumbersome work for our maintenance people to replenish paper towels or clear waste. The design of the Jet Towel also blends into the interior design of our restrooms and improves our restroom ambience."



Factors behind the decision to use the High-speed Hand Dryer:


1. Created a more sanitary environment.
2. Reflects environmental considerations by reducing paper waste.
3. Quicker drying through the Dual Jet airflow.


Background to Installation In use/ Renovated building
Previous drying system Paper towels
Installation sites Restrooms throughout the facility
Shinagawa Prince Hotel

Paperless High-speed Hand Dryer system introduced out of concern for the environment

"Previously, we used paper towels throughout our hotel. But we realised that from an environmental standpoint, a paperless High-speed Hand Dryer simply makes more sense. The dryers also improve restroom appearance, enhance hygiene, and reduce maintenance."



Factors behind the decision to use the High-speed Hand Dryer:


1. Reflects environmental considerations by reducing paper waste
2. Creates a more sanitary environment
3. Quicker drying through dual-jet airflow


Background to Installation New building
Previous drying system Paper towels
Installation sites Restrooms throughout the facility
Number installed 88 units
JR Nagoya Takashimaya

Adding to improved amenities throughout the facility

"We installed the latest High-speed Hand Dryer in all of our restrooms as part of an overall effort to create a more appealing atmosphere for customers. We have found that they really appreciate the convenience of these rapid hand dryers. In addition, because the High-speed Hand Dryer produces no waste, we have been able to present a more environmental image and reduce cleaning costs in the process."



Factors behind the decision to use the High-speed Hand Dryer:


1. Overall improvement in restroom comfort
2. Environmentally-friendly zero-waste system
3. Reduced cleaning and maintenance costs


Background to Installation New building
Previous drying system  -
Installation sites Customer restrooms (men's and ladies' restrooms, shared restrooms)
Number installed 48 units
High-speed Hand Dryer
High-speed Hand Dryer’s many benefits make it suitable for a wide range of environments.