High-speed Hand Dryer
Overview

How It Works

The Jet Towel works much faster than conventional warm-air dryers, completely removing water from the palms and backs of the hands in as little as three to five seconds via dual streams of 382 kilometer-per-hour "jet blasts" of air. All the user need do is insert the hands into the trough and slowly pull them out. Hands will be completely dry, with no hand rubbing or turning required.