Projectors FAQ
Choose a wide-aspect projector
Mitsubishi projectors are going green
FAQ
Q The projector doesn't start when I turn on the power. What could the problem be?
Q Why does the power indicator blink red when I turn on the projector?
Q The power indicator blinks between red and green. What is wrong?
Q The projector is running, but no image is being projected?
Q The projector suddenly stopped projecting the image. What happened?
Why is the image projected distorted?
Q The image projected is blurry. How can this be corrected?
Q There are red/green/blue dots when text is displayed. What's wrong?
Q The image projected on the screen is distorted and a noise is being emitted from the projector. What is the problem?
Q Why is there no sound accompanying the image?
Q Why doesn't anything happen when I try to make adjustments to the projector?
Q Why is there hot air being blown out of the exhaust vents?
line
Q The projector doesn't start when I turn on the power. What could the problem be?
A Check the following:
  • Be sure that the power cord is properly connected to the projector and plugged into the electricity outlet.
  • Turn on the main power switch.
  • Check if the lamp lid is open.
  • The airflow passage may be blocked. Check to see if the air inlet/outlet vents or air filter are clogged with dust or another object. If so, remove/clean the passage.
PAGE TOP PAGE TOP
Q Why does the power indicator blink red when I turn on the projector?
A The reason may be one of the following:
  • The projector was turned on again too soon after it was turned off. Wait for the lighting sequence to correct itself.
  • The power switch was turned off while the fan was running, during or after lamp operation. Repeatedly turn the power switch on and off several times.
  • The room temperature is too high for proper operation.
  • If the lamp is not working, it may be burnt out. Replace it with a new lamp.
PAGE TOP PAGE TOP
Q The power indicator blinks between red and green. What is wrong?
A Check the following:
  • Make sure the filter cover is closed correctly.
  • If either the lamp or temperature indicator is on or blinking, the main unit requires repair. Contact your Mitsubishi Electric dealership.
PAGE TOP PAGE TOP
Q The projector is running, but no image is being projected?
A Check the following:
  • Make sure the lens cap has been removed.
  • Make sure the data source device is turned on and operating properly.
  • Make sure the cables between the data source device and projector are connected correctly.
  • Make sure that the correct input source has been selected.
PAGE TOP PAGE TOP
Q The projector suddenly stopped projecting the image. What happened?
A The projector may have overheated. The airflow passage may be blocked. Turn off the main power switch and check to see if the air inlet/outlet vents or air filter are clogged with dust or another object. If so, remove/clean the passage, and leave the projector turned off for 10 minutes. Turn on the projector and resume.
PAGE TOP PAGE TOP
Q Why is the image projected distorted?
A The projector may not be perpendicular to the screen. Adjust the projector so that it sits at a right angle (90-degrees) to the screen. If the image still seems distorted, try using the Digital Keystone Correction function.
PAGE TOP PAGE TOP
Q The image projected is blurry. How can this be corrected?
A Check the following:
  • The projection distance may be beyond the focus area capability of the model you own. Refer to the specifications in the User's Manual, and adjust the projection distance accordingly.
  • The lens may be dirty. If so, clean it.
  • The image projection size may exceed specifications. Reduce it to between 40-300".
  • Brightness and/or contrast may need correction. Adjust accordingly.
PAGE TOP PAGE TOP
Q There are red/green/blue dots when text is displayed. What's wrong?
A This is a normal condition. There is nothing wrong.
PAGE TOP PAGE TOP
Q The image projected on the screen is distorted and a noise is being emitted from the projector. What is the problem?
A Check the following:
  • The cable from the data source device may not be securely plugged into the projector terminal. Make sure the connecting cable is securely plugged into the terminal.
  • The projector and data source device are located too close to each other. Increase the distance between the projector and data source devices.
PAGE TOP PAGE TOP
Q The image projected on the screen is distorted and a noise is being emitted from the projector. What is the problem?
A Check the following:
  • The cable from the data source device may not be securely plugged into the projector terminal. Make sure the connecting cable is securely plugged into the terminal.
  • The projector and data source device are located too close to each other. Increase the distance between the projector and data source devices.
PAGE TOP PAGE TOP
Q Why is there no sound accompanying the image?
A Check the following:
  • Make sure the volume control is turned on and set at the desired level.
  • Make sure that the cables between the data source device and projector are all connected correctly.
PAGE TOP PAGE TOP
Q Why doesn't anything happen when I try to make adjustments to the projector?
A There may be electrical noise or interference preventing operation of the controls. Press the reset button on the terminal board, and try making adjustments again.
PAGE TOP PAGE TOP
Q Why is there hot air being blown out of the exhaust vents?
A This is part of the equipment cooling process, and is common for projection systems.
PAGE TOP PAGE TOP