|
|
DLP™ systems feature tougher and more reliable chips—resulting in longer lasting liquid crystal systems utilizing an inorganic LCD panel. As a result of focusing on product life—Mitsubishi Electric has selected the highest quality components as well as long-life projection lamps. Using industry-first BrilliantColor™ technology and uniform color reproduction achieves not only compatibility with the international sRGB standard—but also results in high quality image reproduction. Business and education users will enjoy peace of mind with these reliable, quiet-running projectors. DLP™ systems feature tougher and more reliable chips—resulting in longer lasting liquid crystal systems utilizing an inorganic LCD panel. Equipped with our proprietary long life, high pressure mercury lamps—Mitsubishi Electric projectors provide users with peace of mind knowing that their device will be shining brightly for a long time to come.
![]() DLP™ Systems Produce Stable, High Quality Images In the DLP™ system, light does not go through the device. Instead, light is simply reflected off a mirror. This means that dust and dirt cannot penetrate or otherwise affect the device—resulting in even and unchanging color reproduction for years to come.
DLP™ system ![]() DLP™ is a registered trademark of Texas Instruments Applicable Products
Inorganic LCD Panels Make Long Life a Reality Our LCD Panels feature an inorganic orientation membrane and vertically oriented liquid crystal, resulting in longer product lives than those featuring organic orientation membranes. Equipping the device with high-powered lamps does not mean an increase in panel size—the projector features a high level of luminance while remaining compact. Applicable Products
Long Life High Pressure Mercury Lamps Made Possible by Mitsubishi's Proprietary Design Long life lamps are made possible through optimal lamp temperature control design. This design has made possible lamp lives of up to 6000 hours. Extended lamp running times result in reduced costs since lamps won't need to be replaced as often.
*Lamp shown is the VLT-XL650LP (for use with the XL2550U Series) Applicable Products (over max 4000h)
|
|||||||||||||||||||||||||||||||||||||||