Screen Justification Prevents Image Distortion
The projector is able to electronically adjust vertically and horizontally to the correct screen position and does not need to be physically moved (except where rear fixed-focus lens is used). The projector adjusts left and right as well as up and down, so correct screen alignment is made simple. The projector adjusts itself to the environment and is able to handle minute adjustments even when faced with, for example, gusts coming from air conditioning systems. Furthermore, the projector allows for a stacking system to enable projection of overlapping images when two machines are used.
Peace of Mind While Away from the Projector
Simply set up a password to prevent the projector from being used by unauthorized people.
The projector does not need to cool down after being switched off and can be unplugged and either put away or removed.
Featuring a Simple Center Lens Design
The lens is positioned in the center of the projector, so it is easy to align the center of the screen with the center of the projector.
Long-life Lamp Enabling Long-term Reliability
Long life, one of Mitsubishi Electric's signature features, is made possible through optimal design of the lamp temperature control. This means that running costs can be greatly reduced and users can enjoy years of reliable service.
Wireless Connection Possible via Wireless LAN
Computer content projection is possible via wireless LAN connection. Cables that could potentially get in the way are not necessary.
Standby power of less than 1W guarantees economical use of energy.
The projector does not need to be turned around when used on a desk, and can be used simply with its pre-fitted suspension parts when suspended. The lamp is, moreover, easy to replace.
Top loading lamp
Side loading lamp
It is possible to control and monitor the projector remotely via network connection. Moreover, several projectors may be controlled at once.
Equipped with a DVI port to enable high-resolution transmission of digital signals.
Equipped with an HDMI port to enable high-resolution digital images and high-quality sound.
Showing text information in NTSC format (often used in US television broadcasts).
Changing the lamp setting from Normal to Low is possible. Reducing light levels also reduces fan noise, which in turn helps prolong the life of the machine.