Color TFT-LCD Modules for Industrial Use
News
News
News
arrow
2011-07
Mitsubishi Electric Develops 19-inch Super-XGA TFT-LCD Module
Please click for details
arrow
2011-04
Mitsubishi Electric Launches 5-inch WVGA Color TFT LCD Module
Please click for details
arrow
2011-03
Mitsubishi Electric Announces Launch of 8.4-inch Color TFT-LCD Module for Industrial Use
Please click for details
arrow
2010-11
Mitsubishi Electric Launches 9-inch QHD Color TFT LCD Module
Please click for details
arrow
2010-10
Mitsubishi Electric Announces Launch of 5.7-inch Color TFT-LCD Module for Industrial Use
Please click for details
arrow
2010-07
12.1-inch WXGA Color TFT-LCD Modules with LED backlight
Please click for details (89KB) PDF
arrow
2010-06
14.1-inch and 17.5-inch WXGA Color TFT-LCD Modules with LED backlight
Please click for details (160KB) PDF
arrow
2010-04
19.2-inch 1920 x 360 TFT-LCD Module
Please click for details (88KB) PDF
arrow
2010-01
12.1-inch XGA Color TFT-LCD Module with LED backlight
Please click for details (375KB) PDF
arrow
2009-08
15.0-inch Color TFT-LCD Modules for Industrial Use
Mitsubishi Electric has developed two 15-inch TFT-LCD models with a viewing angle of 170 degrees both vertically and horizontally, with a white LED backlight. The white LED backlight does not contain mercury, has high brightness and long life performance and is also inverter-less, which, together, helps reduce the customer's running costs.
Please click for details
arrow
2009-08
Glass Bonding Type Color TFT-LCD Modules for Industrial Use
Mitsubishi Electric introduces 12.1-inch and 15-inch glass bonded color TFT-LCD modules, the main sizes for industrial-use TFT-LCDs, in addition to its current lineup.
Please click for details
arrow
2009-08
Mitsubishi Electric to add Mitsubishi Electric Europe on global network
Mitsubishi Electric Corporation introduces Mitsubishi Electric Europe as a new contact for global network. Mitsubishi Electric will offer even better and local support to Europe area customer.
Please click Global Network for details
arrow
2009-05
9.0-inch COLOR TFT-LCD Modules for Industrial Use
The 9.0-inch wide-VGA LCD modules, which are used for human machine interfaces (HMI), kiosks, home security and other information device applications, will expand Mitsubishi Electric's LCD module offering. For each type of LCD module - with and without touch panels - there is a choice between standard and wide-view models, with the latter having excellent viewing angles from all directions.
Please click for details
arrow
2009-04
Glass Bonding Type Color TFT-LCD Modules for Industrial Use
Mitsubishi Electric will introduce 9-inch, 12.1-inch, and 14.1-inch glass bonded color TFT-LCD module that is wholly bonded by resin to fulfill the outdoor-use products demand with excellent visibility.
Please click for details
arrow
2009-04
15.0-inch Color TFT-LCD Modules for Industrial Use
Mitsubishi Electric already provides 5.7-inch, 6.5-inch, 8.4-inch, 10.4-inch, and 12.1-inch color TFT-LCD modules with LED backlights today. We have developed 15-inch TFT-LCD modules to support applications like ATM.
Please click for details
arrow
2007-09
<Mitsubishi Sales strategy>
Introducing new product family to support our strong growing industrial market.

Mitsubishi has expanded whole new product family to support various demands in industrial market.With our strong industrial market growth, we have developed whole new wide format family and more product sizes for outdoor use application. We are further expanding our global service to support all customers with excellent service.
Please contact our local sales offices for more information on new products.
Learn more...(104KB)PDF
Event News
arrow
2007-10/24-26
Mitsubishi Electric to exhibit at FPD International 2007
Mitsubishi Electric Corporation manufactures and offers high reliability, high quality and environment friendly industrial TFT-LCD modules. Our display provides excellent colorby using our original color conversion Technology Natural Color Matrix. At the Mitsubishi Electric booth, we have new lineups for outdoor use LCD and wide format LCD product family.
Even in high-brightness environments, our Outdoor use LCD shows excellent performance while keeping slim and compact design.

1) Outdoor use LCD
Our high bright LCD emits up to 1500 cd/m2
Transflective LCD achieving both property of transmissivity and reflectivity.

2) Wide Format TFT-LCD Lineup
We have whole new industrial TFT-LCD product family from 4.3 inch WVGA to 17.5 inch WXGA.
arrow
2007-4/11-13
Mitsubishi Electric to exhibit at DISPLAY 2007
Mitsubishi Electric Corporation manufactures and supplies high-reliability and vivid color industrial TFT-LCD modules. These products are designed to withstand tough environments and wide temperature ranges, while displaying vivid colors made possible through our original Natural Color Matrix technology.
At the Mitsubishi Electric booth, we will exhibit our new lineups for outdoor applications and wide format display.

1) Even in high-brightness environments, our slim and compact outdoor use LCDs show excellent performance, emitting up to 1500 cd/m2. We will also be showing our transflective displays that achieve properties of both transmission and reflection.

2) Wide Format TFT-LCD Lineup
Mitsubishi Electric has a whole new lineup of industrial TFT-LCDs from 4.3 inch WVGA to 17.5 inch WXGA.