Global
Company
HOME > Company > CSR > Environmental Topics > Recycling of Waste Plastics > Large-Scale, High-Purity Plastic Recycling

Environmental Topics

Recycling of Waste PlasticsRecycling of Waste Plastics

Large-Scale, High-Purity Plastic RecyclingLarge-Scale, High-Purity Plastic Recycling

Aiming for 100% Closed-loop RecyclingAiming for 100% Closed-loop Recycling

When plastic that has been recovered from used home appliances is recycled, it is typically recycled into knick-knacks, imitation wood and other such products, a process called downgrading. However, this also means that resources must be continually consumed. What is really needed is closed-loop recycling—recovering plastics from old products and recycling it in new products.

Hyper Cycle Technology for Closed-loop Recycling

Hyper Cycle Technology for Closed-loop Recycling

Conventional plastic recycling is usually limited to plastic parts made of a single material that is easy to separate out. Moreover, separating and recovery are conducted manually, so only around 10% of the plastic can be retrieved from the recycled product; the remainder is incinerated or landfilled.

In order to make it possible to create products out of 100% recycled materials instead of new materials, Mitsubishi Electric took on the challenge of automatically separating, recovering and recycling recyclable materials taken from shredded mixed plastic, a material that had traditionally proven difficult to recycle.


Japan's very first large-scale, high-purity plastic recycling systemJapan's very first large-scale, high-purity plastic recycling system

The main types of plastic used in home appliances are polypropylene (PP), polystyrene (PS) and acrylonitrile-butadiene-styrene (ABS). Mitsubishi Electric has succeeded in accurately separating mixtures of these plastics at purity levels exceeding 99%. This high degree of purity is made possible by proprietary technologies for separating different plastics by specific gravity and by electrostatic properties. PP, which is lighter than water, can be separated out using technology for separating by specific gravity, whereas ABS and PS, which are heavier than water and cannot be isolated in this way, are separated using differences in their electrostatic properties. (See the next page for details on these separating technologies.)

Large-Scale High-Purity Recycling at Material Recycling Plant

Previously, we recycled approximately 600 tons of plastic in Mitsubishi Electric home appliances, out of a total of approximately 10,000 tons generated by our home appliance recycling plant, Hyper Cycle Systems Co., Ltd, a ratio of just 6%. Now, thanks to successfully developing high-purity separating technologies, we recover approximately 6,400 tons of the three major plastics for recycling in our home appliances in a closed-loop system. This represents Japan's very first large-scale high-purity plastic recycling system.

Reducing CO2 emissions by 6,700 tons annuallyReducing CO2 emissions by 6,700 tons annually

Comparison of CO2 Emissions from Plastic Manufacturing

Promoting the "3Rs" (reducing, reusing and recycling) for home appliances is one of the pillars of Mitsubishi Electric's Environmental Vision 2021. Our large-scale high-purity plastic recycling system recycles the three major plastics in a closed loop from shredded mixed plastic. The system reduces use of these three major plastics by our home appliances business by around 18%. This translates into less new plastic produced, which in turn reduces carbon dioxide by 6,700 tons annually (Mitsubishi Electric estimate). The kind of closed-loop recycling pioneered by Mitsubishi Electric will be a driving force behind eliminating waste and preventing global warming.


Topics
Successfully Developed Technology for Rapidly Removing a RoHS Regulated Substance from Shredded Mixed Plastic

Plastic mixtures being separated for recycling sometimes contain flame-retardant plastics with very small amounts of high-density bromine. However, compliance with the EU's RoHS Directive is a critical part of recycled plastics in home appliances. Currently, flame-retardant plastic is removed by utilizing its high specific gravity and setting a low specific gravity to separate out compliant varieties. With this method, however, it is exceedingly difficult to increase the amount of plastic recovered. But, in February 2009, Mitsubishi Electric succeeded in developing a new technology for rapidly and automatically detecting and removing brominated flame retardants from PP, PS and ABS. In 2010 we plan to apply this technology to mass production lines at our home appliance recycling plant.

Mechanism of Large-scale mass production plant
*
RoHS Directive: An EU directive on the Restriction of the Use of Certain Hazardous Substances in Electrical and Electronic Equipment. Restricts use of six types of hazardous substances: lead, mercury, cadmium, hexavalent chromium, polybrominated biphenyls and polybrominated diphenyl ether. Cadmium content must be less than 0.01 wt% (content percentage on same substance basis); the other substances must have a content percentage of less than 0.1 wt%.