Font Size:
Company

R&D / Technology – Water Treatment Technology based on a Membrane Bioreactor using Ozonated Water

Water Treatment Technology based on a Membrane Bioreactor using Ozonated Water

High-speed filtration of municipal and industrial wastewater
Realizes energy savings and compactness in water treatment equipment

  • Industry
  • Energy Savings
  • Compactness
  • : Indicates R&D category.
  • : Indicates purpose, feature or effect of the R&D.

Overview

Eco-MBR
ZOOM

Mitsubishi Electric has developed an immersion-type membrane bioreactor that uses ozonated water to clean the membrane filter (the Eco-MBR*1). The unit realizes high-speed filtration with approximately twice the flow rate of permeate per unit of membrane surface area, halving the number of membrane filters required, increasing compactness, and reducing energy consumption by 25%*2 compared to conventional membrane bioreactors.

Technology Point

Issues with conventional immersion-type membrane bioreactors

Conventional immersion-type membrane bioreactor, Mechanism of membrane filtration and cleaning
ZOOM

Immersion-type membrane bioreactors separate activated sludge and treated water using a membrane filter immersed in activated sludge. Continued filtration results in the membrane filter becoming clogged with foulants, increasing pressure loss. In conventional immersion-type membrane bioreactors, the filter foulants are removed and the filter is cleaned by supplying a sodium hypochlorite solution from the opposite direction of filtering. However, since the membrane filter is more prone to become clogged the greater the speed of filtration, it has not been possible to realize high-speed filtration using sodium hypochlorite, which has a limited cleaning effect. In addition, it is necessary to supply a high flow rate of air bubbles from the lower section of the membrane filter in order to scour activated sludge adhering to the membrane surface, and this significantly increases energy consumption.

The Eco-MBR: Effective removal of filter foulants

Cleaning the membrane filter using ozonated water
ZOOM

The developed Eco-MBR uses ozonated water to clean the membrane filter. Ozone demonstrates 1.4 times the oxidation power of sodium hypochlorite. In addition, increasing the concentration of the ozonated water enables effective removal of filter foulants using less water and less ozone.

Superior energy-saving performance contributes to the realization of a sustainable water-recycling society

Increased energy-saving performance of Eco-MBR
ZOOM

The Eco-MBR efficiently removes foulants from the membrane filter through repeated washing with ozonated water, reducing the time required for the same amount of water to pass through the membrane. This makes it possible to realize high-speed filtration, and to halve the number of filters employed. As a result, the flow rate of air supplied to the lower section of the membrane filter for cleaning the membrane surface can be halved, which will save energy. The application of the Eco-MBR in the recycling of municipal and industrial wastewater will contribute to the realization of sustainable water-recycling societies both in Japan and throughout the world.

*1
Eco-Membrane BioReactor
*2
Mitsubishi Electric figures
Page Top