Education and support

e-learning courses (English)

A collection of frequently used FA terms and example sentences! FA field glossary

Choose from download edition or pdf.
See "Using the download edition data" at the bottom of this page for methods of expanding the data in the download edition.

Using the download edition data

English

CoursesPCPC/TabletPDF
FA Equipment for Beginners PLCs All Courses
HMIs
Inverters
Servos
Industrial Network
Positioning
Process Control System
Industrial Robots
Power Distribution Control Products -
Basic edition / Advanced editions Programmable Controllers MELSEC-iQ-R/Q/L/FX MELSEC iQ-R Series Basics -
MELSEC-Q Series Basics -
MELSEC iQ-F Series Basics -
MELSEC-L Series Basics -
GX Works2 Basics -
GX Works2 Advanced -
GX Works3 (Ladder) -
PLC Programing Basic (ST) -
PLC Programing Basic (Ladder) -
Applications of Programming -
Efficient Programming -
CC-Link IE Controller Network -
CC-Link IE Field Network -
CC-Link IE Field Network
(MELSEC iQ-R Series)
-
CC-Link -
Ethernet -
Intelligent Function Module -
Intelligent Function Module
(MELSEC iQ-R Series)
-
Serial Communication -
Positioning -
MELSEC Process Control System Basics -
PLC System Maintenance -
Safety CPU Basics(iQ-R) -
Safety Controller Basics -
Human-Machine Interfaces(HMIs)-GOT GOT Basics (GT16, GT Designer3) -
Inverters-FREQROL FREQROL Basics 800 (Operation) -
FREQROL Basics 800 (Function) -
FREQROL Basics 800 (Maintenance) -
FREQROL Basics (Operation) -
FREQROL Basics (Function) -
Inverter energy saving course -
AC Servos-MELSERVO MELSERVO Basics (MR-J4) -
MELSERVO Basics
(MR-J4-GF Servo Amplifier I/O Mode) NEW
-
MELSERVO Basics
(ME-JE Modbus)
-
SIMPLE MOTION Module
(iQ-R)
-
SIMPLE MOTION Module
(iQ-R CC-Link IE Field)
-
SIMPLE MOTION Module
(iQ-F)
-
SIMPLE MOTION Module -
MOTION CONTROLLER Basics
(Hardware)
-
MOTION CONTROLLER Basics
(Real Mode:SFC)
-
MOTION CONTROLLER Application
(Virtual Mode)
-
Linear Servo -
Industrial Robots-MELFA MELFA Basic and Maintenance
(FD Series)
-
MELFA Basic and Maintenance
(FQ Series)
-
Power Distribution Control Products Low-Voltage Circuit Breaker -
Contactors and Motor Starters -

Using the download edition data

[How to expand the downloaded file]
Download the file to a folder of your choice.
When you decompress the downloaded file, a folder will be created.

Decompression method 1) When using an OS that features a ZIP-compatible decompression tool (Windows Vista / 7 / 8 )
Right click on the downloaded file.
Select "Expand All".
Specify the expansion destination, and click on the "Expand" button to decompress the file.
If "Expand All" is not displayed, use decompression method 2) below.

Decompression method 2) When using an OS which does not feature a ZIP-compatible decompression tool
If your OS does not feature a ZIP-compatible decompression tool, please obtain a decompression tool separately.
Use the decompression tool to decompress the file.
Decompress the file to a directory.
* The user accepts full responsibility for the use of a decompression tool.

[How to start]
Double click on "exe file" in the folder that has been created, and a menu screen will appear. Select the desired model from the menu screen.