Motion controller System Configuration
Q173DSCPU/Q172DSCPU
System Configuration
- The Q-series Motion controllers can configure a Multiple CPU system with Programmable controllers.
- By selecting the Motion CPU and PLC CPU according to the application, a flexible system is configured.
- The Multiple CPU system is capable of using up to four CPU modules. (one PLC CPU must be used.)
- Over 100 types of Q series modules are available, which enhances system scalability.
- Up to 96 axes of servo motors can be controlled by using three modules of the Q173DSCPU.
- (Note-1): Destination of the external input signals (FLS, RLS, DOG) can be changed with parameters.
- (Note-2): Be sure to use the cable for forced stop input (sold separately).
- (Note-3): Motion modules (Q172DLX/Q172DEX/Q173DPX) cannot be installed in CPU slot and I/O slot 0 to 2 of the main base unit.
- (Note-4): Install Q172DEX to the main base unit. Do not install to the extension base unit.
- (Note-5): It is impossible to mount the main base unit by DIN rail when using the Motion CPU module.
- (Note-6): Use the Graphic Operation Terminal (GOT) compatible with Motion CPU (Q173DSCPU/Q172DSCPU). When you use GOT2000, refer to the "GOT2000 Series
Connection Manual (Mitsubishi Products)". When you use GOT1000, refer to the "GOT1000 Series Connection Manual (Mitsubishi Products)".