• twitter
  • facebook
  • mail

Products

Print Page

 

Conveyor Tracking Application

Vision cameras detect workpieces on conveyors.
Workpieces are transported and aligned by robots without stopping conveyors.

Introduction advantages

Mitsubishi provides hardware, software, and supporting tools as a package to make designing, programming, and startup on tracking system configuration by customers easy. Introduction advantages

No more complex wiring!

  • Devices and cables required for tracking are packaged.
  • Wiring is completed only by connecting connectors.
  • Hands and vacuum solenoid valves for hands have already been installed to robots as default.
Easy wiring

Easy startup with just 5 steps!

  • Easy startup with wizard format (interactive format) of dedicated tools (No manuals are required. Just touch buttons following messages shown in the screen.)
  • No need to create robot programs
  • No more complex communication settings and parameter settings (automatic setting)
  • Calibration of conveyors and vision sensors is also completed only by following instructions on the wizard.
  • Startup adjustment can be easily performed in the wizard format!
*Teaching operation is required in the calibration screen.

Easy startup

High-accuracy and high-speed operation can be performed!

  • Synchronization performance of vision recognition and conveyor speed is improved by the new high-speed input function.
  • Dedicated programs optimized for tracking with higher speed and higher accuracy are installed.