![]()
![]()
From A/V Enthusiasts to Web Surfers, New 1999 MCEA Products Deliver High Performance to Broad Range of Consumers
LAS VEGAS, May 8, 1998 - Programmable VCRs with advanced editing capabilities, a second generation DVD player, a "Theater in a Box" and a new WebTV® Plus receiver are just a few of the new products unveiled today by Mitsubishi Consumer Electronics America, Inc. (MCEA) at its annual Dealer Line Show.
"While many consumers equate Mitsubishi with high performance televisions, most people don't realize we offer other consumer electronics products with the same quality for a superb home theater system," explained Suketaka Tachibana, chairman of Mitsubishi Consumer Electronics America, Inc. "Whether a person enjoys viewing or editing movies, listening to music or surfing on the Internet, chances are they will be interested in one or more of the new products in our 1999 lineup."
VCRs
Mitsubishi Consumer Electronics America’s new line of VCRs offer higher
performance, easier operation and attractive new designs. The company’s VCRs
are available in two series, standard and deluxe, and offer a wide range of
features targeted to all levels of A/V enthusiasts.
Standard VCRs have suggested retail prices from $249-$379 and include the HS-U140, HS-U431, HS-U440 and HS-U540. The HS-U440 and HS-U540 feature Super Quasi Playback™, enabling the VCR to play S-VHS recorded tapes without having to purchase an S-VHS VCR. These two models also feature faster mechanisms, enabling the VCRs to rewind a T-120 cassette in 86 seconds and provide picture search at 27 times its play speed.
Additional Standard line features include:
Deluxe Line VCRs
Mitsubishi Consumer Electronics America's new Deluxe line of VCRs include
advanced editing capabilities and Super-VHS performance. With suggested retail
prices from $429-$749, Deluxe model VCRs include the HS-U590, HS-U681, HS-U781
and HS-U790.
The HS-U681 is engineered for consumers who dub and edit segments from other VHS tapes. It features a flying erase head for noise-free transitions between recorded segments, an edit jack for communication between play and record units, and pre-roll cueing. It also offers Movie Advance, which automatically fast forwards pre-recorded movie tapes to the beginning of the actual movie.
The HS-U781 is one of two S-VHS VCRs in MCEA’s line. S-VHS recordings have lower noise and wider video bandwidth than conventional VHS recordings. The HS-U781 also features a digital comb filter for improved color separations, S-Video passthrough, enabling the VCR to be connected in line between a satellite box and TV, and a front panel S-Video input jack.
The top-of-the-line HS-U790 combines the S-VHS capabilities of the HS-U781 with the editing features of the HS-U681. This includes the flying erase head, an edit jack for communication between play and record units, pre-roll cueing and an audio recording level control.
Additional features on Deluxe VCRs include:
DVD Player
MCEA's second-generation DVD player, the DD-2000, is an ideal solution for
consumers looking to add superior video and audio quality to their home
theaters. The DD-2000 is designed for playback of movies, operas, plays,
concerts and other full-motion video programs as well as conventional and 96kHz
audio CDs.
With a suggested retail price of $799, the DD-2000 offers high-performance video processing for a crisp, clear picture and higher performance audio processing for superb sound quality and compatibility to future digital audio recordings. Upgraded features in the DD-2000 include a 20-bit/96kHz sampling rate audio processor, 108 dB audio signal/noise ratio, 96 dB audio dynamic range and 0.004% audio distortion (THD).
The DD-2000's remote control codes are stored in new Mitsubishi TV remotes, enabling single remote operation of an entire A/V system. The rear panel digital audio bitstream output jack provides a Dolby® Digital Surround or PCM Linear signal for decoding in an external processor or A/V receiver.
Home Theater Components
The M-TS401 "Theater in a Box" is a complete home theater surround
audio system in one package. With a suggested retail price of $799,
"Theater in a Box" is easy to set up and combines MCEA’s SP-401
matching six-piece speaker system with the M-VR400 Dolby® Pro Logic®
A/V receiver and 100 feet of 18-gauge speaker wire. The system provides true
high-fidelity performance when listening to television or radio broadcasts and
has inputs for connection to a CD player and cassette deck.
Still available in MCEA’s 1999 line up are other top quality audio components essential for a complete home theater system such as:
MCEA also introduced the WB-2001 WebTV® Plus Receiver with added upgrade capacity over the company’s introductory receiver, the WB-2000. This set-top box receiver enables users to access the Internet by connecting their television to an existing telephone line.
About Mitsubishi Consumer Electronics America
Mitsubishi Consumer Electronics America, Inc. (MCEA) manufactures and markets a
comprehensive line of premium quality, high definition-upgradable and projection
televisions, VCRs and audio products for complete home theater systems.
Recognized as the world leader and innovator of big screen and digital
television receiver technology, MCEA develops audio and video products that lead
the industry in performance, ease-of-use and system integration. For additional
information about MCEA, visit http://www.mitsubishi-tv.com.
*Editor’s Note: VCR Plus+ and C3 are registered trademarks of Gemstar Development Corporation. The VCR Plus+ system is manufactured under license from Gemstar Development Corporation and VCR Index Systems B.V., respectively. WebTV is a registered trademark of WebTV Networks, Inc. Dolby and Pro Logic are registered trademarks of Dolby Laboratories Licensing Corporation.
For more information:
MEA News Bureau
800/828-6372 for media use only