![]()
![]()
Mitsubishi Electric Slashes Microwave/RF Amplifier
Design Time with New "Design Accelerator Kit"
for SMD High-Power GaAs FET Family
Includes DataSurveyor Processing Software
That Provides
Graphical View of Actual In-Circuit MGF09XXA Device Performance
SUNNYVALE, Calif. February 12, 2002 To give design engineers the fastest possible way of starting microwave and RF power amplifier designs, the Electronic Device Group of Mitsubishi Electric & Electronics USA, Inc., has launched a new software-based Design Accelerator Kit for its MGF09XXA family of SMD High-Power GaAs FETs. A significant upgrade from the starter kit announced in May 2001, the new Design Accelerator Kit features Mitsubishi Electrics DataSurveyor processing software, which enables designers to graphically view a MGF09XXA devices in-circuit performance data throughout the familys 0.5- to 6-GHz frequency range a giant leap beyond synthesized performance data.
The Design Accelerator Kit comes equipped with a CD-ROM containing the DataSurveyor software, samples of each device in the MGF09XXA family, two reference boards (one fully tuned and one untuned), and reference designs for several single-stage and push-pull amplifier applications.
The kit currently showcases the MGF0915A, the familys highest-powered product at 36 dBm, mounted on a fully tuned board for the 2.5- to 2.7-GHz frequency range. The MGF0915A is a popular choice for applications such as tower-top antennas and customer premise equipment in the Multichannel Multipoint Distribution Service (MMDS) and Wireless Local Loop (WLL) frequency bands.
The DataSurveyor software included with the kit enables engineers to mathematically process and manipulate performance data for a MGF09XXA device to learn its optimal operational characteristics in an actual circuit. Engineers can use this data to quickly validate anticipated device performance over several different drive and biasing conditions.
The reference boards offer the unique feature of being machine-assembled application circuits that are tunable using special zero-ohm resistors as jumpers. Combining this jumper capability with electromagnetic modeling software enables engineers to turn around their designs with fewer or no iterations, hastening the process from design conception to production and making routine the characterization of discrete components and their associated footprints.
"We developed the Design Accelerator Kit to give design engineers everything they need to perform meaningful design work in as few as 10 minutes," said Bryon Gutow, senior product marketing manager for microwave and RF products at Mitsubishi Electric & Electronics USA, Inc. "We continue to provide customers with whatever tools we can to reduce or eliminate design obstacles."
Availability
Mitsubishi Electrics new Design Accelerator Kit is available now for the MGF09XXA High-Power GaAs FET family.
# # #
About Mitsubishi Electric & Electronics USA, Inc.
Mitsubishi Electric Corporation manufactures a diverse range of microwave and RF semiconductors for linear, low-noise and high-power communications applications, including satellite and terrestrial transmitters and receivers, marine and vehicular mobile radios, cellular phones and subscriber units. The company produces gallium-arsenide (GaAs) FETs, HBTs, MICs, MMICs and HEMTs; silicon RF power transistors and modules; and surface acoustic wave (SAW) filters for the industrial and consumer markets. Mitsubishi Electric markets its microwave and RF semiconductors in North America through the Electronic Device Group of Mitsubishi Electric & Electronics USA, Inc.
Mitsubishi Electric Corporation and its North American affiliate, Mitsubishi Electric & Electronics USA, Inc., are world-class suppliers of semiconductors and electronic products for communications, industrial, Internet-enabled, automotive, and visual applications. Mitsubishi combines its systems-level expertise and high-level silicon process technologies to provide chip, chipset and system-on-chip solutions. The company is ranked among the top-tier worldwide semiconductor suppliers and offers an extensive range of semiconductor and computer system components for the North American marketplace, including DRAM, flash, SRAM, ASIC, ASSP, MCU, microwave/RF, and optoelectronic devices.
Additional information on the Mitsubishi Electric Semiconductor Group is available at http://www.mitsubishichips.com.
Trademark Information
Mitsubishi and the Mitsubishi logo are registered trademarks of Mitsubishi Electric Corporation in the USA, Japan, and other countries. DataSurveyor is a trademark of Mitsubishi Electric & Electronics USA, Inc. All other companies and products referenced herein are trademarks or registered trademarks of their respective holders.
Keywords
Mitsubishi, microwave, RF, GaAs, FET, amplifier, field effect transistor, high frequency, semiconductor.
For More Information:
Positio Investor & Public Relations
Dave Richardson
(650) 815-1006, Ext. 108
dave@positiopr.com
Mitsubishi Electric & Electronics USA, Inc.
John Garner
(408) 774-3191
garner_john@edg.mea.com