![]()
![]()
Mitsubishi Electrics New 32-Bit Automotive MCU Offers
Industrys Largest Flash Memory Capacity
SUNNYVALE, Calif. October 2, 2002 The Electronic Device Group of Mitsubishi Electric & Electronics USA, Inc., furthered its commitment to the North American automotive market by introducing two M32R/ECU 32-bit microcontrollers designed for high-end, controller area network (CAN) automotive applications, such as engine control, airbag system, and EV (motor control), as a cost-effective, high-performance alternative to microprocessors. The new devices, dubbed the M32R/ECU#5 (M32180 Group) and M32R/ECU#5HL (M32182 Group), offer up to 1 Mbyte of flash memory the industrys largest flash capacity incorporate a more advanced M32R floating point unit (FPU) core, boost clock speed up to 80 MHz, and operate throughout a wide temperature range (-40 to +125 degrees C).
"Mitsubishi Electrics M32R/ECU microcontrollers are an industry leader in on-chip flash memory capacity, and the latest generation of devices continues that tradition," said Richard Sessions, director of embedded systems at Mitsubishi Electric & Electronics USA, Inc. "Adding the FPU and doubling the processing speed accelerates performance to a microprocessor level in high-end automotive systems for a more cost-effective value. Mitsubishi Electric accelerated the process of debugging code with our new JTAG Interface With Tracing development tool, so customers can get to market faster."
Powerful M32R-FPU Core
The new generation of devices incorporates an FPU into Mitsubishi Electrics original
compact M32R 32-bit high-performance RISC core. The new core is fully IEEE 754
compliant for single-precision operations and supports all exceptions defined in the IEEE
754 specification. The FPU greatly boosts the operation-speed performance of the new M32R
microcontrollers, reducing single-precision instruction time by 95 percent and cutting in
half the execution time of double-precision instructions, compared to previous-generation
devices. The core also executes most frequently used instructions in one clock cycle, as
well as compound instructions that execute two operations in one cycle.
The M32R-FPU core is capable of high code efficiency because its instruction set accommodates 16-bit and 32-bit instructions. The FPU incorporates multiply-accumulate and difference-of-products instructions that are suitable for Fast Fourier Transform (FFT) butterfly computation, as well as DSP-function instructions for the built-in multiplier-accumulator.
In addition, the M32R-FPU core supports a wide logical address space of 4 Gbytes without requiring segment switching, thus resulting in higher computational efficiency.
Large-Capacity Flash Memory
The new M32R/ECU devices offer large DINOR flash memory capacity to increase productivity
at the development of manufacturing stages, and to contribute to improved maintainability
in the field. The M32R/ECU#5 offers 1,024 Kbytes of flash memory with 48 Kbytes of
RAM, and the M32R/ECU#5HL offers 384 Kbytes of flash memory and 64 Kbytes of
RAM. Both devices offer memory expansion, which allows designers to add external discrete
memory capacity.
Mitsubishi Electrics DINOR flash memory enables customers to program using a single 3.3- or 5.0-volt power supply. Designers can program quickly at a rate of 64 Kbytes every two seconds, regardless of the operating frequency. The devices support serial programming or software-based CPU programming as well as block erase and collective erase modes, giving designers more flexibility. The flash memory even provides a security function that protects against unauthorized readout or modification by any third party.
JTAG Interface With Tracing Development Tool
The new M32R/ECU devices incorporate a special tracing tool into the JTAG interface to
streamline the code debugging process. The tool captures many clock cycles of code
execution history so that designers can quickly narrow a coding problem to its source and
make corrections, enabling faster time-to-market development.
Broad Development Tools Support
The M32R/ECU family is supported by proprietary and third-party development tools, such as
system modeling software, real-time operating systems, C code generators, debugging and
data calibration, and flash programming tools.
Packaging and Availability
Mitsubishi Electrics M32R/ECU#5 microcontroller is available in a 240-pin QFP
package. Samples will be available in June 2003 with volume production scheduled for March
2004.
The M32R/ECU#5HL microcontroller is available in a 144-pin QFP package. Samples will be available in February 2003 with volume production scheduled for September 2003.
# # #
About Mitsubishi Electric & Electronics USA, Inc.
Mitsubishi Electric Corporation is a top-10 semiconductor supplier and ranks among the
top-five worldwide suppliers of 8- and 16-bit microcontrollers. The company designs and
manufactures powerful embedded MCU platforms for embedded industrial control, automotive,
consumer entertainment, and communications applications. Mitsubishi Electrics MCU
products include the number one global selling 16-bit, M16C platform a
feature-rich, low-noise, ultra-low power, and code-efficient core that easily scales
across customers end-product lines. The company also offers 8-, 16-, and 32-bit
point solution MCU platforms including USB; Flash-Over-USB; CAN; LIN; and keyboard,
battery, and LCD control.
All Mitsubishi Electric semiconductor global manufacturing facilities, engineering design centers, and marketing and sales centers supplying MCU products to the automotive industry are QS-9000 certified. Mitsubishi Electric is a founding member of EEMBCthe Embedded Microprocessor Benchmark Consortiumand is a member of the USB Implementers Forum and the Smart Battery Implementers Forum. The company markets its microcontroller products in North America through the Electronic Device Group of Mitsubishi Electric & Electronics USA, Inc.
Mitsubishi Electric also offers an extensive range of semiconductor and system components for the North American marketplace, including optoelectronic, microwave/RF, ASIC, ASSP, and memory ICs and modules. Additional information on the Mitsubishi Electric Semiconductor Group is available at www.mitsubishichips.com.
Trademark Information
Mitsubishi and the Mitsubishi logo are registered trademarks of Mitsubishi Electric
Corporation in the USA, Japan, and other countries. All other companies and products
referenced herein are trademarks or registered trademarks of their respective holders.
Keywords
Mitsubishi, M32R/ECU, M32R, 32-Bit, CAN, microcontroller, MCU.
For More Information:
Mitsubishi Electric & Electronics USA, Inc.
John Garner
(408) 774-3191
garner_john@edg.mea.com
Positio Investor & Public Relations (for Mitsubishi Electric)
Dave Richardson
(650) 815-1006, Ext. 108
dave@positiopr.com