Mitsubishi Electric US Companies

News Release - For Immediate Release

 

Mitsubishi Electric Introduces New Hi-Speed USB 2.0 Peripheral Controller to Complement Full Range of USB Devices

PC Peripheral, Audio-Visual, and Mobile Applications Benefit from Small Package Size,
Battery-Saving Power Management Function

SUNNYVALE, Calif. — December 10, 2002 — The Electronic Device Group of Mitsubishi Electric & Electronics USA, Inc., announced it has further extended its Universal Serial Bus (USB) device family with the introduction of its USB 2.0-compliant M66591GP USB Peripheral Controller. Designed for use with an external processor, the device provides both Hi-Speed (480-Mbps) and Full-Speed (12-Mbps) control, bulk, and interrupt USB transfers for PC peripherals such as hard disk and CD-ROM drives, printers, and scanners as well as audio-visual applications like set-top boxes.

Mobile applications that require Hi-Speed functionality, such as digital still cameras and digital video cameras, also benefit from the M66591GP because of its compact 0.4-mm pitch, 10-mm by 10-mm, 80-pin LQFP package; a power management function that conserves battery life; and a 1.8- or 3.3-volt interface power source.

The device can deliver bulk transfers at Hi-Speed and features a built-in USB transceiver, a multi-function high-speed bus interface, an independent 8-bit split bus (DMA interface) as well as a separate/multiplex selectable 16-bit CPU bus. It also has a built-in 3.5-Kbyte FIFO for data buffering and a maximum of seven endpoints for data transfer. Each endpoint is optimized by transfer type, transfer direction, and FIFO memory size. The device not only meets the USB 2.0 standard, but has also passed the USB Compliance Test.

"The M66591GP complements our existing line of USB devices, extending us beyond Full-Speed into the Hi-Speed application space," said George Riehm, senior marketing manager for consumer products at Mitsubishi Electric & Electronics USA, Inc. "With this new device, we now have a range of products that are optimized for any application, depending upon speed requirements and data transfer size."

The M66591GP is the latest in a family of USB devices catering to the growing demand for PC and peripheral data transfer capability. Mitsubishi Electric now offers multiple USB 2.0-compliant devices that deliver Full-Speed or Low-Speed (1.5-Mbps) data transfer rates for wide range of peripherals.

Availability
Mitsubishi Electric’s M66591GP begins sampling in January 2003, with volume production scheduled for the second quarter of 2003.

# # #

About Mitsubishi Electric & Electronics USA, Inc.
Ranked among the top-tier worldwide semiconductor suppliers, Mitsubishi Electric Corporation is a leading manufacturer of application-specific standard products (ASSPs) for motor driver, TV, VCR, fax, disk drive, telephone, communications, and audio/video system applications, as well as standard linear and digital/analog interface ICs. Mitsubishi Electric's ASSPs are manufactured with extensive feature sets that meet specific application requirements and use a standard-cell design approach to reduce chip size, costs, and product development time. The company implements its ASSPs as standard ICs for multiple customers and maps them to singular or multiple applications.

Mitsubishi Electric offers an extensive range of semiconductor-based products and markets them to the North American marketplace through the Electronic Device Group of Mitsubishi Electric & Electronics USA, Inc.

Additional information on the Mitsubishi Electric Semiconductor Group is available at http://www.mitsubishichips.com/.

Trademark Information
Mitsubishi and the Mitsubishi logo are registered trademarks of Mitsubishi Electric Corporation in the USA, Japan, and other countries. All other companies and products referenced herein are trademarks or registered trademarks of their respective holders.

Keywords
Mitsubishi, USB, USB 2.0, Hi-Speed, USB controller, USB peripheral, Universal Serial Bus.

For More Information:

Positio Investor & Public Relations (for Mitsubishi Electric)
Dave Richardson
(650) 815-1006, Ext. 108
dave@positiopr.com

Mitsubishi Electric & Electronics USA, Inc.
John Garner
(408) 774-3191
garner_john@edg.mea.com 

Customer Contact:
(408) 774-3189
customerservice@edg.mea.com

 


Close Window