![]()
![]()
Mitsubishi Electric Simplifies MCU Migration Path to More Powerful Performance with New Ultra-Power-Efficient 16-Bit Platform Microcontroller
Platform Design and Flash Reliability Are Key to Meeting Customer Requirements
SUNNYVALE, Calif. October 7, 2002 As market migration from 8- to 16-bit microcontrollers (MCUs) continues to gather pace, the Electronic Device Group of Mitsubishi Electric & Electronics USA, Inc., launched the M16C/26 (M3026x), an ultra-low power MCU for powerful, yet power-sensitive applications. The M16C/26 offers 16-bit peripherals and performance up to 20 megahertz (MHz) at 8-bit price ranges for consumer, industrial and automotive control applications. In line with the current easy-to-use, powerful M16C family of 16-bit platform MCUs, the new flash-based MCU has high C-code efficiency, excellent EMI/EMS performance, and complete code and pin compatibility with other M16C Platform MCUs. The M16C/26 is the first of a new series of MCUs targeting power management, instrumentation, point-of-sale, remote security, three-phase motor control, and meter applications where high processing performance, powerful peripherals, and low power consumption are key factors.
"There is a definite shift occurring right now in the MCU market to more powerful and flexible processors," said Richard Sessions, director of embedded systems for Mitsubishi Electric & Electronics USA, Inc. "Our platform design allows easy and cost-effective transition to 16-bit performance at 8-bit prices. The M16C/26 offers highly reliable flash ROM and virtual data EEPROM for applications that demand performance."
By integrating a sophisticated voltage down converter, the M16C/26 is capable of operating at full rated 20-MHz speed with ultra-low power consumption across a wide voltage range of 3.0 to 5.5 volts (10 MHz at under 3.0 volts). This is particularly key for applications that require high processing capability at low voltages such as gas, water, and electric meters and remote security systems.
In addition to the migration to more powerful 16-bit processors, the MCU market is seeing a shift from mask to flash-based MCUs as flash versions reach value parity and allow much more design flexibility, which significantly improves product time-to-market.
Mitsubishi Electrics M16C flash MCUs are widely used in many "mission critical" applications including automotive safety, industrial control, communications, and computing systems. They use an extremely robust proprietary Hyper New DINOR flash technology that is not affected by process variations. This is achieved by creating memory cells with enough margin in operations and characteristics to eliminate bit failures and by setting in-process screening steps to remove defect-induced data retention failures. In addition, all M16C flash MCUs are capable of 100,000 erase/write cycles (typical).
"With tens of millions of flash devices in service, we have had no flash ROM bit failures from the field. You can use M16C flash MCUs in complete confidence, without fear of failure or more expensive manufacturing due to flash reliability issues," added Sessions.
Packaging and Availability
Mitsubishi Electrics M16C/26 is available in a compact, 7-mm x 7-mm, 48-pin QFP
package. Samples of the M16C/26 and StarterKit Plus development tools are available
now, with volume production scheduled for the first quarter of 2003.
M16C/26 Notable Features:
# # #
About Mitsubishi Electric & Electronics USA, Inc.
Mitsubishi Electric Corporation is a top-10 semiconductor supplier and ranks among the
top-five worldwide suppliers of 8- and 16-bit microcontrollers. The company designs and
manufactures powerful embedded MCU platforms for embedded industrial control, automotive,
consumer entertainment, and communications applications. Mitsubishi Electrics MCU
products include the number one global selling 16-bit, M16C platform a
feature-rich, low-noise, ultra-low power, and code-efficient core that easily scales
across customers end-product lines. The company also offers 8-, 16-, and 32-bit
point solution MCU platforms including USB; Flash-Over-USB; CAN; LIN; and keyboard,
battery, and LCD control.
All Mitsubishi Electric semiconductor global manufacturing facilities, engineering design centers, and marketing and sales centers supplying MCU products to the automotive industry are QS-9000 certified. Mitsubishi Electric is a founding member of EEMBCthe Embedded Microprocessor Benchmark Consortiumand is a member of the USB Implementers Forum and the Smart Battery Implementers Forum. The company markets its microcontroller products in North America through the Electronic Device Group of Mitsubishi Electric & Electronics USA, Inc.
Mitsubishi Electric also offers an extensive range of semiconductor and system components for the North American marketplace, including optoelectronic, microwave/RF, ASIC, ASSP, and memory ICs and modules. Additional information on the Mitsubishi Electric Semiconductor Group is available at www.mitsubishichips.com.
Trademark Information
Mitsubishi and the Mitsubishi logo are registered trademarks of Mitsubishi Electric
Corporation in the USA, Japan, and other countries. M16C and StarterKit Plus are
trademarks of Mitsubishi Electric & Electronics USA, Inc. All other companies and
products referenced herein are trademarks or registered trademarks of their respective
holders.
Keywords
Mitsubishi, M16C, microcontroller, MCU, 16-bit.
For More Information:
Mitsubishi Electric & Electronics USA, Inc.
John Garner
(408) 774-3191
garner_john@edg.mea.com
Positio Investor & Public Relations (for Mitsubishi Electric)
Dave Richardson
(650) 815-1006, Ext. 108
dave@positiopr.com