Mitsubishi Electric US Companies

News Release - For Immediate Release
 

Mitsubishi Electric Automation introduces next-generation plc

FX3U is most advanced and capable compact logic controller

 

VERNON HILLS, Ill. – September 29, 2006 – Mitsubishi Electric Automation, Inc., a major supplier of industrial automation equipment, has introduced its FX3U Series line of next-generation SuperMicroTM programmable logic controllers that offer unmatched execution speed, performance-enhancing instructions and unparalleled connectivity. The new devices, which are backward-compatible to Mitsubishi Electric’s FX2N series, are available now, including relay and transistor base units, software and most peripherals.

 

Ideal for nearly any machine control application, the FX3U delivers faster throughput, larger memory (800 per cent more than the previous series), improved motion integration and broader network connectivity. Unlike rack-based platforms that have separate power supplies, CPUs and input/out modules, the FX3U compact PLC integrates all of these components in a single platform. What’s more, the FX3U has the most memory and fastest instruction processing time of any PLC in its class, and is the only compact PLC with a Profibus Master and a high-speed fiber optic networking card for servo amplifier control.

 

The FX3U also features left- and right-hand buses for communication, analog I/O, and high-speed input and high-speed output modules, which further increases system flexibility and application opportunities.

 

“Our engineers added a host of robust, evolutionary improvements in the FX3U to expand the range of applications and increase performance,” said Ken Doner, FX and Alpha series product manager at Mitsubishi Electric Automation. “The FX3U has up to eight times more memory than other compact PLCs, and because it can handle more functions, will ultimately result in cost-savings.”

 

The FX3U is available through Mitsubishi Electric’s North American distributor network, which can be accessed at http://www.meau.com, or by calling 847.478.2100.

 

About Mitsubishi Electric Automation, Inc.
Mitsubishi Electric Automation, Inc., a U.S. subsidiary of Mitsubishi Electric Corporation of Japan, supplies factory automation solutions such as programmable logic controllers, human-machine interfaces (HMI), programming and control software, variable frequency drives, motion products including computer numerical controllers (CNC) and servo controls. Mitsubishi Electric has sales and service facilities throughout North and South America that support pre-sale application support and post-sale service requirements. Mitsubishi Electric serves a broad range of industrial markets, applications and customers including the automotive, wood, machine tool, semiconductor, textile and commercial markets, and applications such as material handling, packaging, printing and specialty machinery.

 

For more information, visit http://www.meau.com.

 

# # #

 

Contact

Lori Bacharz

Mitsubishi Electric Automation, Inc.

847.478.2417

bacharzl@meau.mea.com
 

About the FX3U Compact PLC from Mitsubishi Electric Automation

 

Hardware Features

·         Huge 64K steps (128kB) standard user memory – 800% increase from FX2N

·         384 physical I/O mixed between local and network (256 local I/O maximum)

·         Up to 300% increase in device range

·         Distinct new Left Hand (LH) and improved Right Hand (RH) communication buses increase system flexibility and application range

·         The RH bus supports faster communication to existing FX2N modules

·         The RH bus supports new FX3U modules (SSCNET 3, Ethernet, Profibus DP)

·         The LH bus supports New Slim-Line Adapter Modules and existing FX2N adapters

·         100 kHz counting on each of six base-unit high-speed inputs

·         100 kHz pulse train output capability on each of the three base-unit transistor outputs for three-axis pulse-type motion control from a transistor base unit – without extra modules

·         Low-cost, high-speed I/O adapter (RH bus) to handle pulse-type motion on relay base units

·         Add up to three serial port adapters per CPU. Options include RS232, RS485 and USB

·         Real-time clock embedded in the base unit (no optional cassette needed)

·         Optional CPU-mounted display panel supports text messages, device monitor and data editing

·         New full-function FX3U Ethernet module (FX3U-ENET)

·         New Profibus DP Master Module (FX3U-64DP-M)  

·         New SSCNET III two-axis optical network module supports MR-J3 servos (FX3U-20SSC-H) 

 

System Features

·         Exceptional Execution Speed - can exceed FX2N by 200-500% (200% speed increase is  typical)

·         Improved Network Connectivity

·         Master/peer capability: Ethernet, CC Link, CC Link/LT, Profibus DP, AS-I and FX-Net

·         Local/Slave capability: Ethernet, CC Link, Profibus DP, FX-Net

·         Complete OPC connectivity including Ethernet (MX OPC Server v4.10 or higher)

·         Embedded commands for Mitsubishi Electric Freqrol inverters (VFDs)

·         Reference SFM data devices directly in programs (eliminates pre/post data handling)

·         FX3U Intelligent (SF) modules support direct CPU access for improved ease-of-use

·         Software Configuration Utilities (like many advanced platforms)

·         Retains parameter access in the logic program to facilitate on-the-fly setup changes

·         Improved ASCII string handling features

·         Improved floating point math features

·         Instruction set approximates Q-Series to facilitate migration