![]()
![]()
Sierra Nevada Brewery Taps Mitsubishi Electric for Solar Power
CYPRESS, Calif. — January 15, 2008 — Mitsubishi Electric & Electronics
USA, Inc. has been selected to provide photovoltaic (PV) panels for the Sierra
Nevada Brewery in Chico, Calif. The 1.3 megawatt system is being installed in
two phases by Chico Electric and will provide 34 percent of the brewery’s power.
“Sierra Nevada Brewery is one of the most environmentally conscious companies in
the industry and we are honored to be working on this project with them.” says
Gina Heng, director of marketing for Mitsubishi Electric & Electronics USA’s
Photovoltaic Division. In addition to the new solar electric system, the brewery
has installed a 1MW fuel cell, a 500 kW solar array shade structure in its
parking lot, and it also makes methane from brewery waste products, all part of
an effort to use clean energy and make the brewery energy independent.
Mitsubishi Electric is providing 6,800 of its 185Wp high-strength,
corrosion-resistant modules for the project. The modules contain no lead solder,
a technology Mitsubishi Electric introduced to the United States in 2005.
Instead of lead-solder coating for the cells, Mitsubishi Electric developed
silver electrodes that offer superior weatherproofing and higher PV module
conversion efficiency.
Chico Electric completed the first phase of the project on Dec. 31, 2007. The
next phase will be finished in June, 2008 after construction of a new building
on the brewery’s property.
“We are proud to have the opportunity to design and install a solar electric
system for such a forward-thinking company like Sierra Nevada Brewery. We feel
this project is a good match for us given our extensive background in electrical
services and the brewery’s commitment to the environment,” says Norm Nielsen,
president of Chico Electric.
About Mitsubishi Electric & Electronics USA’s Photovoltaic Division
Mitsubishi Electric is one of the world’s largest manufacturers and providers of
solar power technology. The company’s eco-friendly photovoltaic systems are used
throughout the world to bring clean, reliable energy to residences, business,
power generation plants, schools, factories and areas without access to
electricity, as well as other applications such highway and stadium lighting. In
the United States, Mitsubishi Electric photovoltaic panels are marketed by
Mitsubishi Electric & Electronics USA, Inc., and sold only through authorized
distributors and installers. For more information visit
www.mitsubishielectricsolar.com or call 714.220.2500.
About Chico Electric
Chico Electric has been in business since 1960 and has grown to be a leading
electrical contractor in California. Chico Electric designs and installs solar
electric systems for commercial and residential customers, and offers a wide
range of high quality electrical services through their construction department,
agricultural services department, and quick services department.
# # #
CONTACT:
Jenean Smith
Mitsubishi Electric & Electronics USA, Inc.
Photovoltaic Division
5665 Plaza Drive
Cypress CA 90630
(714) 220-6861
Jenean.smith@meus.mea.com
Norm Nielsen
Chico Electric
36 W Eaton Road
Chico, CA 95973
(530) 891-1933 x.202
nnielsen@chicoelectric.com