BackPrint

News Release Archives

Note that the releases are accurate at the time of publication but may be subject to change without notice.

FOR IMMEDIATE RELEASE No.2548

Mitsubishi Electric Installs Diamond Vision Screen at Boat Race Fukuoka

1,513-inch screen becomes second largest display at a Japanese boat racecourse

Tokyo, September 6, 2010 - Mitsubishi Electric Corporation (TOKYO: 6503) announced today that it has completed installation of a Diamond Vision large-scale display system at Boat Race Fukuoka in Fukuoka, Japan. The new 1,513-inch screen, replacing the previous CRT screens installed in 1996, is the second largest display at a Japanese boat racecourse and the largest in the Kyushu area.

The new screen, which displays high-definition video content, incorporates high-luminance light-emitting diodes (LEDs) aligned vertically and horizontally in a 15-millimeter dot pitch and the latest digital screen controllers. The display system faces the main stand across the racing surface, and will flexibly display a variety of programs such as dynamic live race videos, contestant profiles, odds, order of arrival and other gaming information.
Boat Race Fukuoka's New Diamond Vision Screen

Boat Race Fukuoka's New Diamond Vision Screen

Specifications

Product name Diamond Vision LED
Screen size 36 m (w) x 13.44 m (h); 483.84 m2; 1,513-inch
Light emitting element High luminance LED element (red, blue and green)
Dot pitch
Pixel size (dot) 2,466 (w) x 946 (h)

Inquiry