News Release Archives
Note that the releases are accurate at the time of publication but may be subject to change without notice.
Mitsubishi Electric Completes Installation of Diamond Vision Screen at Marine Messe Fukuoka
9 x 5 m screen to provide business and leisure video content

The screen incorporates the latest high definition digital screen controllers and high luminance light-emitting diodes (LEDs) aligned in a 6 mm pixel pitch. The new screen replaces the facility's current, main CRT display, also built and installed by Mitsubishi Electric Corporation in 1995. The company's Arena Easy-to-use Operator Console feature allows facility operators to easily display video content extracted from a PC or handycam. Mitsubishi Electric Corporation completed the installation of the system, including the new screen, video equipment system and live cameras, at the end of January 2011.
Marine Messe Fukuoka, operated by the Foundation of Fukuoka Convention Center, opened in 1995. The versatile facility is used for exhibitions, athletic functions, conferences and concerts. Mitsubishi Electric has recently installed numerous other Diamond Vision displays worldwide, which include the following:
・ 800-inch display at Hiratsuka Stadium in November 2010
・ 1513-inch display at Fukuoka Kyotei (boat racing) in August 2010
・ 600-inch display at Kumamoto's KKWING in March 2010
・ 700-inch display at Toda Kyotei (boat racing) in March 2010
・ 1,036-inch display at Kleenex Stadium Miyagi (baseball) in March 2010
 659-inch display at the Hakodate Racecourse paddock area in February 2010
・ 4,255-inch display at Dubai's Meydan Racecourse in January 2010
・ Two 2,086-inch displays and two 695-inch displays at Cowboys Stadium in September 2009
Mitsubishi Electric aims to further expand its business in large scale displays for public facilities.
Specifications
|
Inquiry
Mitsubishi Electric Corporation