BackPrint

News Release Archives

Note that the releases are accurate at the time of publication but may be subject to change without notice.

FOR IMMEDIATE RELEASE No.2578

Mitsubishi Electric PV System to Power Makita's Diesel Engine Factory

85kW system to partially cover manufacturing, air conditioning and ighting requirements at main factory

Tokyo, February 21, 2011 - Mitsubishi Electric Corporation (TOKYO: 6503) announced today that it has installed an 85-kilowatt (kW) photovoltaic (PV) system on the roof of Makita Corporation's main factory in Takamatsu City, Japan. The PV system, which is the first for Makita, comprises PV modules, inverters and other equipment, and will begin generating electricity later this month.

Electricity generated by a total of 448 PV modules installed over a surface area of 700 square meters will cover approximately 3 percent of the manufacturing, air conditioning and lighting requirements at Makita's marine diesel engine factory. The installation is expected to generate approximately 94,730 kilowatt-hours (kWh) of electricity annually, and will help reduce environmental impact through the use of renewable energy, exemplifying Makita's commitment towards creating a low-carbon society.
Mitsubishi Electric PV System installed on the roof of Makita's main factory

Mitsubishi Electric PV System installed on the roof of Makita's main factory

Inquiry