BackPrint

News Release Archives

Note that the releases are accurate at the time of publication but may be subject to change without notice.

FOR IMMEDIATE RELEASE No.2614

Mitsubishi Electric Develops 19-inch Super-XGA TFT-LCD Module

Tokyo, July 14, 2011 - Mitsubishi Electric Corporation (TOKYO: 6503) announced today it has developed a 19-inch Super-XGA color TFT-LCD module built for rugged performance in a wide range of outdoor-signage applications.
19-inch Super-XGA TFT-LCD Module(AA190EA01)

AA190EA01

The module boasts 1,500cd/m2 super-high brightness, 100,000-hour service life durability at an environment temperature of 25 degrees Celsius and a market-leading operating-temperature range of between -20 degrees and 70 degrees Celsius. In addition, high-voltage inverters are not required for operation. The module is also fully compliant with the European Restriction of the use of certain Hazardous Substances in electrical and electronic equipment (RoHS) directive, and is completely mercury-free.


The display, which Mitsubishi Electric believes is the world's first Super-XGA TFT-LCD measuring 19 inches, will begin selling on October 1 through the following Mitsubishi Electric offices: http://global.MitsubishiElectric.com/bu/tft_lcd. Initial production has been set at 1,000 units per month.


Going forward, Mitsubishi Electric plans to further expand its lineup of industrial TFT-LCD modules, which now come in 14 screen sizes.


TFT-LCDs increasingly are being used for digital signage in a variety of environments and applications, raising the demand for models offering extra brightness, durability and heat/cold resistance for outdoor uses. At the same time, end-users are demanding ever larger screens and higher resolutions to display as much information as possible on one screen.

Specifications

Model Number AA190EA01
Display size (resolution) 19-inch (1280 × 1024 dots)
Display Area (mm) 376.32 (H) × 301.056 (V)
Dots 1280 (H) ×1024 (V)
Pixel Pitch (mm) 0.294(H) × 0.294 (V)
Contrast Ratio 800: 1
Luminance (cd/m2) 1,500
Viewing Angles (CR>10)(°) -80 +80 (H); -80 +80 (V)
Colors 262K (6 bits/color)
16.77M (8 bits/color)
Backlight Unit LED
Electrical Interface LVDS 6/8bit
Dimensions (mm) 404.2 (W) × 330.0 (H) × 14.9 (D)
Operating Temperatures (°C) -20 70
Storage Temperatures (°C) -30 80

Inquiry