BackPrint

News Release Archives

Note that the releases are accurate at the time of publication but may be subject to change without notice.

FOR IMMEDIATE RELEASE No.2618

Mitsubishi Electric to Sell 1.3-Micrometer Band 40Gbps EML Module

Tokyo, August 30, 2011 - Mitsubishi Electric Corporation (TOKYO: 6503) announced today the coming launch of a compact 1.3-micrometer band 40Gbps Electro-Absorption Modulator Laser (EML) module for optical signal transmission of up to 10 kilometers by devices used for sending large-volume data. The FU-497SEA, which will launch commercially on November 1, will be presented during the 13th China International Optoelectronic Exposition (CIOE) at Shenzhen Convention and Exhibition Center in Shenzhen, China on September 6-9.

As online traffic continues to increase at rapid pace, 10Gbps optical interfaces for networks are giving way to faster 40Gbps interfaces. Mitsubishi Electric's existing 40Gbps EML module, the FU-697SEA, uses the 1.55-micrometer band for transmissions that are limited to about two kilometers due to wavelength dispersion. As chromatic dispersion at 1.3 micrometers is almost negligible, Mitsubishi Electric's new 1.3-micrometer band EML chip delivers high signal quality for 40Gbps optical transmissions over distances of up to 10 kilometers.
FU-497SEA

FU-497SEA

Main Features

High signal quality for transmissions of up to 10km
-Transmission penalty is less than 1dB after 10km using single-mode fiber
-High extinction ratio (10dB, typical) and high mask margin (10%, typical) at 43Gbps operation
Use of general-purpose interface for 40Gbps electrical connection
-Dual SMPM connectors for differential connection between modules and digital signal circuits help to simplify system designs for transmission equipment

Other Features

Other Features

Modulation format: NRZ

Light emission central wavelength: 1.3-micrometer band

Output power: 0 to 4 dBm

Maximum transmission distance: 10km

Package: XLMD-MSA compliant

Input (RF signals): dual SMPM connectors with differential signal interface

Output (optical signal): LC connector with a single mode fiber


Going forward, Mitsubishi Electric plans to introduce additional compact, power-saving EML modules.

Inquiry