BackPrint

News Release Archives

Note that the releases are accurate at the time of publication but may be subject to change without notice.

FOR IMMEDIATE RELEASE No. 3176

Mitsubishi Electric Develops Compact Hardware AI for Implementation on Small-scale FPGAs

Improved real-time processing and reduced costs will expand opportunities for AI deployment in home appliances, elevators, high-precision maps and more

TOKYO, February 14, 2018 - Mitsubishi Electric Corporation (TOKYO: 6503) announced today it has developed a compact hardware artificial intelligence (AI) technology that can be implemented on small-scale field programmable gate arrays (FPGAs) that users and designers can configure to develop tailored applications. Mitsubishi Electric leveraged its Maisart*-brand AI technology to achieve a solution that uses a highly efficient calculation order and optimized circuit architecture for improved real-time processing and reduced costs, which is expected to expand the scope of AI deployment in home appliances, elevators, high-precision maps and more.

* Mitsubishi Electric's AI creates the State-of-the- ART in TechnologyMaisart
Envisioned applications for Mitsubishi Electric's Maisart-brand

Key Features

1) Compact AI enables fast real-time processing in FPGAs
-Improved calculation-order efficiency and optimized circuit architecture for FPGA implementation.
-Reduces inference computations to one-tenth** the time of conventional AI and improves real-time processing.
** Compared to Mitsubishi Electric's existing technology that implements conventional deep learning on FPGAs
2) Compact, small-scale circuit architecture will expand usage of AI in FPGAs
-Miniaturized circuit architecture realizes compact AI for implementation in small-scale FPGAs, as well as embedded CPUs, for reduced costs and energy consumption.
-Small-scale FPGA implementation will broaden scope of AI application in home appliances, elevators, high-precision maps and other products/fields where AI usage has been limited by high costs.

Development Summary

  Processing time on the same scale FPGA FPGA scale required for the same level inference Bands/standards
Proposed Compact AI on FPGA Short(1/10th of conventional time**) 3
Conventional Technology 12 dB 35% 1

Inquiry