The New York Times Personal Technology  
-
NYTimes: Home - Site Index - Archive - Help Welcome, rugbypr - Member Center - Log out
-
 
Search:

HOW IT WORKS; And You Thought Your Neighbor Had a Jumbo TV


By MICHEL MARRIOTT
Published: December 23, 2004

LIKE a lost scene from Ridley Scott's futuristic cult movie ''Blade Runner,'' Times Square soars with glittering buildings that pulse and wink with outsized video screens.

A little more than a decade ago, there was only one, the Sony Jumbotron, which anchored the southern end of the square. Now billboard-size screens are commonplace. The newest went into service last month. Its designer, Mitsubishi Electric Power Products' Diamond Vision division, says it is one of the largest outdoor full-color high-definition video screens in the world.

Mounted in a giant picture frame on Seventh Avenue between 44th and 45th Streets, the screen is 21 feet 5 inches high by 37 feet 9 inches wide and about 4 feet deep, although most of the depth is taken up by the catwalks used to service it. With a screen area of about 800 square feet, it's about 80 times bigger than the largest home TV's.

The screen, across Times Square from the glass-walled studios of MTV, the Viacom division that owns it, can broadcast music videos, news, content from MTV's Web site and live events taking place in the studio and elsewhere.

Next month, an interactive feature will be added: pedestrians will be able to use their mobile phones to play along with programs on the screen, including text-message-based video games. And MTV executives say they are considering ways to enable viewers to hear the screen's offerings as well, either over low-power radio broadcasts or by dialing a special number on a cellphone.

Akira Tasaki, president and chief executive of Mitsubishi Electric U.S., said the high-definition display, which at its core consists of more than two million light-emitting diodes, is among his company's most technologically sophisticated screens.

For one thing, because it is a true high-definition screen -- like more and more of the fanciest sets sold for home use -- it displays images at 1080i resolution, meaning it paints the screen with 1,080 lines in two passes -- interlaced -- 30 times a second. That's more than twice the number of lines a standard-definition screen has. Each of the 1,080 lines in the HDTV screen consists of 1,920 pixels, the smallest element of an image.

At the scale of the MTV screen, those pixels are created by a bouquet of L.E.D.'s that can be controlled to produce any color. On the MTV screen, the L.E.D.'s are closely arranged in a quad pattern of two red dots, one green and one blue.

This arrangement becomes important, said David Corathers, the engineering manager for Diamond Vision, because it permits the screen to manipulate dots, creating a sort of intermediate dot he calls a dynamic pixel. This, Mr. Corathers said, helps to render sharper pictures than typical L.E.D. screens display.

The screen also requires ''fewer pixels to create something that looks much, much higher in resolution,'' Mr. Corathers said.

Another digital technology, called color space conversion, compensates for and corrects the tendency of large L.E.D. screens to produce oversaturated colors, making, for instance, red appear more like hot pink.

The screen's specially color-tuned L.E.D.'s are mounted in a panel called a lighting unit. The lighting units are then arranged 34 high by 30 wide to create the screen that has a 16:9 aspect ratio, sometimes known as letterbox.

The units also have custom-made louvers, removable eyelids of sorts that can be used to improve the screen's viewing angle and that help maintain contrast even in bright sunlight. Like most outdoor video screens, the MTV screen has to be viewed in varying lighting conditions.

While many large L.E.D. screens are driven by off-the-shelf personal computers that process their content, Mark Foster, general manager for Diamond Vision, said the MTV screen uses high-capacity custom processors linked to MTV's studios by a fiber-optic cable.


OUR ADVERTISERS



Stop Spyware Today! Webroot Spy Sweeper


Up to 15% off new Dell Home systems. Click for details.