Product Features Long-term SupportProduct Features Long-term Support

Design Compatibility

Successful support within the industrial market requires long-term product support.

Mitsubishi Electric is focused upon providing a long-term steady supply of products in addition to product support service.

Even when current models are discontinued, Mitsubishi Electric will offer a new model with improved functionality while ensuring compatibility with the current model.

Design Compatibility


Long-life LED Backlight

The lifetime of a TFT-LCD module backlight is generally required to perform in industrial applications for 7 or more years.

Mitsubishi Electric offers long-life TFT-LCD modules with LED backlights that have a lifetime of 100,000 hours.*1*2*3

*1:
Mitsubishi Electric defines lifetime of LED as the point that its brightness deteriorates to 50% of its initial value.
*2:
The lifetime of a lamp is greatly affected by changes of ambient temperature, and is shortened in high temperature especially.
*3:
Excluding the following displays - AA043MA01, AA050MG01, AA050MG02, and AA150XS11