Home Appliances
Energy-saving Heating Control for Air to Water System
Heating control that learns and utilizes the thermal characteristics of buildings.
Contributes to improved comfort and increased energy saving.
Overview
We have developed a hot water heating control technology for an Air to Water (ATW) Heat Pump System installed in homes across Europe.
This ATW system distributes hot water produced by the heat pump to each room in order to warm up the entire house. Our new technology realizes hot water heating control that responds to thermal characteristics that differ from building to building, realizing both comfort and energy saving.

Technology Point
Learns the different thermal characteristics of each building


The thermal characteristics of buildings such as thermal insulation performance are improving year by year, but differ greatly depending on when the building was constructed. Older buildings therefore require a flow of high-temperature water in order to maintain a comfortable room temperature (e.g. 20°C), while newer buildings require lower temperature water. Our research modeled the relationship between water temperature, outside temperature, and room temperature, and developed a thermal characteristic learning algorithm able to learn the thermal characteristics of a building such as heat dissipation characteristics and time constants from heat pump operation data.
Determines water temperature with consideration of thermal characteristics

Our new hot water heating control technology determines the optimal water temperature depending on fluctuations in the outside temperature and the room temperature, with consideration of the thermal characteristics of the building. It improves responsivity when the thermostat setting is changed, and reduces room temperature fluctuations after the set room temperature is reached, increasing comfort for occupants. In addition, the reduction of unnecessary heat pump operation increases the efficiency of heat pump operation, improving energy-saving performance.
Verification of effectiveness at HVAC evaluation facility using mock-up houses in Scotland
The effect of this development is verified at our facility named "House-type HVACS Evaluation Facility" in Scotland.

- About
- Locations
- History
- Corporate data
- Organization
- Purpose
- Management policy
- Corporate strategy
- President’s message
- Procurement activities
- R&D / technology
- ADVANCE magazine
- Intellectual property
- Research
- Maisart
- ClariSense
- SUSTIE
- Technology videos