Initiatives that contribute to addressing social issues

Semiconductor & Device Group

Message from the Group President

Contributing to the Realization of a Decarbonized Society by Providing Energy-Efficient Products, Key Devices for Customers, in Response to Energy and Environment-related Social Issues

photo: Yuzuru Saito

Yuzuru Saito
Executive Officer, Group President, Semiconductor & Device

The Semiconductor & Device Group provides semiconductors and devices that play a key role for home to space appliances and enrich our living. We recognize energy and environmental issues as today's social issues and contribute to the realization of a sustainable society by providing low-power products to customers.

In order to achieve carbon neutrality, a requirement for sustainable societies, it is imperative to use generated power while minimizing power loss in the process. Power semiconductor devices are incorporated into a number of power electronics such as EVs and air conditioners, playing a significant role in reducing power loss. In addition, Mitsubishi Electric manufactures state-of-the-art products using silicon carbide (SiC).

The Semiconductor & Device Group provides today’s society, where DX is underway, with high-performance, low-power, compact high-frequency devices and optical devices for wireless communications equipment, optical fiber communications, and data centers that make full use of multiple semiconductor technologies. Furthermore, by reducing the space required for communications equipment, the cooling function can be simplified, thereby contributing to comprehensive energy savings.

As described above, the Semiconductor & Device Group is taking part in the achievement of carbon neutrality and the realization of a sustainable society by providing key devices for overcoming energy and environmental limitations while driving forward the digital revolution in the post-pandemic society.

Major social issues for which risks and opportunities have been recognized and evaluated Priority SDG initiatives
  • Appropriate use of water
  • Proper management of chemical substances
  • Addressing climate change
  • Preservation of biodiversity
icon: Priority SDG initiatives

Initiatives that Contribute to Addressing Social Issues

SiC Power Semiconductor Devices that Achieve Low-Power Consumption of Customers' Devices

  • icons: SDGs #13 Climate Action
photo: Second-generation full SiC power module for industrial use

Second-generation full SiC power module for industrial use

From the viewpoint of energy savings and environmental protection, Mitsubishi Electric is developing semiconductor devices using silicon carbide (SiC)*1, the material physical attributes of which can significantly contribute to reducing power loss, and expanding the product lineup.
In fiscal 2011, we were the first company in the world to equip air conditioners with SiC power semiconductor modules. Since then, we have promoted their use in various products such as rolling stock and industrial equipment. In January 2021, we launched a newly developed power semiconductor module that is the second-generation full SiC power module for industrial use. With the SiC-MOSFET*2 and SiC-SBD*3 chips, this new module reduces power losses by approximately 70% compared to our conventional Si-IGBT module. By expanding the lineup, it contributes to improving the efficiency, reducing the size, and lighter electric vehicle power supply systems used for charging batteries, photovoltaic power systems, air conditioners, and more.
We will continue to accelerate the development of new technologies and products to respond to diverse needs for energy efficiency.

  1. *1 SiC: Silicon Carbide (a compound of silicon and carbon)
  2. *2 MOSFET: Metal Oxide Semiconductor Field Effect Transistor
  3. *3 SBD: Schottky Barrier Diode

Optical Communication Device that Contributes to Low Power Consumption of Network Equipment for 5G Mobile Communications Base Stations

  • icons: SDGs #13 Climate Action
photo: 100Gbps EML CAN

100Gbps EML CAN

Data transmission volume has been rapidly increasing with the widespread use of handheld mobile communication devices and the storage of information on cloud networks. In response to these trends, the construction of large-volume, high-speed optical communications systems is being planned between base stations where traffic is concentrated and exchanges where communication signals from base stations are centrally controlled. In October 2020, Mitsubishi Electric started to offer samples of the industry's first 100Gbps*1 EML*2 CAN*3, a new optical communications device that is used to connect the base stations in such networks. It improves the speed and volume of mobile communications systems and reduces energy consumption, thus contributing to energy efficiency.

  1. *1 Gbps (Gigabits per second): Unit of communication rate. 1Gbps indicates that 1 billion digital codes can be transmitted per second.
  2. *2 EML (Electro-absorption Modulated Laser diode)
  3. *3 CAN (TO-CAN): Package with excellent productivity (mass production capacity) widely used in optical communications devices.