Download

Print Page

Controllers - Computerized Numerical Controllers(CNCs) Dimensions/CAD

About copyright, and the operating environment, notes

Spindle Motor

SJ-VL Series

loading..

[Copyright]

Mitsubishi Electric Corporation

[How to use]

  • 1. Select one of the underlined models from the table above. Then, download the DXF file with the product model name in the next screen.
  • 2. Import the DXF file into your CAD software.
    Mitsubishi Electric has confirmed that the CAD software below reads the DXF files.
CAD softwareCompany
AUTO CAD LT2007Autodesk Inc.
  • 3. Because DXF files are intermediate files, the data is not fully compatible.
    Some CAD software may not read the files completely. 
  • 4. These DXF files were created in millimeters.