Solutions
Logistics

RGV/AGV
Operation monitoring and predictive maintenance
- Real-time data collection by network-connected FA devices
- Processing and analysis of onsite data by using edge computing products
- Cooperation with e-F@ctory alliance partners
Solutions to the Issues
| Issues | Solutions |
|---|---|
| Avoidance of slip effect during high-speed operation and stop | High response and high precision by combining multiple encoders positioning implementation |
| Multi wheel drive control | Multi-axis simultaneous operation with simple position command for one axis |
| Fast start-up | Program simplification by using function blocks |
| Miniaturization of RGV/AGV | Space saving by utilizing multi-axis amplifier |
System Configuration

feature
Avoidance of slip effect during high-speed operation and stopFully Closed Control
High response and high precision by combining motor side and load side encoder for positioning
In operation: servo motor side, In stop: Position control by switching to machine side encoder. High gain setting becomes possible. The settling time is shortened and the influence of the slip of the driving section is eliminated, enabling high-precision positioning control.

How to Configure Full Closed Control
By using Engineering tool MELSOFT GX Works3 fully closed control electronic gear setting for the servo parameter of axis 1.
[MELSOFT GX Works3 Fully Closed Control Setting Screen]
Multi wheel drive controlMaster/Slave operation
Multi-axis torque sharing operation with position command for one axis
Since the MR-J4-B can transmit the same torque data from the master axis to the slave axis through driver communication, multi-axis torque sharing operation is possible

Setting of master/slave operation
Set servo parameters corresponding to master and slave axes with engineering tool MELSOFT GX Works3.
[MELSOFT GX Works3 master/slave operation setting screen]
Fast start-upFunctfion Blocks
Program simplification by using function blocks (FB)
With the unit FB of MELSOFT GX Works3, motion control such as positioning control and advanced synchronization control can be programmed easily.

Programming with Function Blocks
With engineering tool MELSOFT GX Works3, you can create a program simply by dragging and dropping the necessary FB from the unit FB or registered FB provided on FA site to the editor screen.
[MELSOFT GX Works3 Program Creation Screen]
Miniaturization of RGV/AGVMulti-Axis integrated servo amplifier
Space saving realized by utilizing multi-axis amplifier (MR-J4W)
Space saving while maintaining servo amplifier performance