FA Application Package iQ Monozukuri Deburring / Polishing Application

Perkenalan
Easily creates a machining path of deburring/polishing and performs machining.
On-site operators can automate their teaching process with rough teaching using a master workpiece and tools. (Supported robots: RV-F series)
*Mar 31, 2024 to be discontinued.

Advantages
- On-site operators can create a machining path at their sites.
- Teaching can be easily performed wiht the simple configuration.
- Compared with the offline teaching that uses an actual workpiece, the statup time has decreased by 80%.