iQ Monozukuri PACKAGING Packaging Library
- Four types of mechanisms
- Compensation function of packaging film
- Workpieces compensation function (Alignment conveyor)
Four types of mechanisms
Cams used for the following four types of mechanisms are generated with the cam auto-generation function.
| Rotary cutter
|
Box motion *
|
| Long dwell
|
Flying shear
|
- * Only the MELSEC iQ-R series Simple Motion module is supported.
Compensation function of packaging film
A deviation is calculated based on the mark detection data and compensated with a control of the auxiliary axis.
Workpieces compensation function (Alignment conveyor)
Workpieces on the conveyor are aligned at predetermined intervals.