Stand-Alone Motion Controller System Configuration
Q170MSCPU
System Configuration
- (Note-1): Destination of the external input signals of servo amplifier (FLS, RLS, DOG) can be changed with parameters.
- (Note-2): Be sure to use the cable for forced stop input.
- (Note-3): Use the Graphic Operation Terminal (GOT) compatible with Q170MSCPU(-S1).
When you use GOT2000, refer to the "GOT2000 Series Connection Manual (Mitsubishi Products)".
When you use GOT1000, refer to the "GOT1000 Series Connection Manual (Mitsubishi Products)".