Coolant is used for cooling the inside of the inverter. Liquid cooling enables new applications in the environments where heat is difficult to be dissipated.
A smaller enclosure can be used since the quantity of the heat dissipated in the enclosure is reduced.
A sensor (flow switch) is attached at the inlet of coolant to send a signal to the inverter. When the coolant flow rate decreases, a warning is output, enabling quick, direct detection of system faults.
The power supply voltage of 690 VAC is supported. A wider range of power supply voltage is covered.
The FR-A800-E-LC inverter can be remotely operated via Ethernet using FR Configurator2, which will be upgraded soon. Parameter setting, monitoring, and maintenance (for example, parts lifespan diagnosis) of the FR-A800-E-LC inverter is possible through network. Adjustment time and downtime of the inverter can be reduced.
■Inverter
■DC reactor