Factory Automation

Safety Sub-Functions Compliant with IEC/EN 61800-5-2

MR-JET-G4-HS supports safety sub-functions, STO/SS1/SBC/SLS/SSM/SDI/SLT.

Safe torque off
(STO)

Responding to the input signal from external equipment, the STO function shuts off power to the servo motor electronically using the internal circuit (shuts off through secondary-side output). This function corresponds to the Stop category 0 of IEC/EN 60204-1.

Safe torque off (STO)

Safe stop 1
(SS1)

Responding to the input signal from external equipment, the servo motor starts to decelerate. After the set delay time for motor stop is passed, the STO function starts. Monitoring the servo motor deceleration based on the motor deceleration rate is also supported. This function corresponds to the Stop category 1 of IEC/EN 60204-1.

Safe stop 1 (SS1)

Safe brake control
(SBC)

The SBC signals are outputted for external brake control.

Safe stop 2 (SBC)

Safely-limited speed
(SLS)

This function monitors the speed of the servo motor not to exceed the specified speed limit. If the speed exceeds the limit, the motor power is shut off by the STO.

Safely-limited speed (SLS)

Safe speed monitor
(SSM)

The SSM signals are outputted when the speed of the servo motor is below the specified speed limit.

Safe speed monitor (SSM)

Safe direction
(SDI)

This function monitors whether the servo motor moves in the command direction. If the servo motor moves in a different direction from the command direction, the STO function is executed.

Safe direction (SDI)

Safely-limited torque
(SLT)

This function monitors the torque (or the thrust) of the servo motor not to deviate from the specified range. If the torque (or the thrust) exceeds the range, the STO function is executed.

Safe direction (SDI)
  : Function activation area