Energy Saving Supporting DevicesMES3-EAP1-AI Specifications

Specifications
Category | ||
Group | ||
Model | ||
Product name | ||
Model name | ||
Measuring point settings | Register collection source | |
Collection source | ||
Number of collection sources | ||
Number of measuring points | ||
Register manual input measuring point | ||
Register product type time period measuring point | ||
Measuring value point Time period measuring point |
||
Register calculation measuring point | ||
Available measuring point | ||
Register specific consumption measuring point | ||
Energy measuring point Production number measuring point |
||
Graph function | Analysis method (Graph type) |
|
Display interval | ||
Dashboard function | Dashboard creation | |
Available panel | ||
Display mode | ||
Display settings | Auto-update | |
Tab display | ||
Auto-switch | ||
HTML output | ||
Report function | Format | |
Saving number of report settings | ||
Number of output items | ||
Output item | ||
Report creation | Daily report | |
Monthly report | ||
Annual report | ||
Automatic report output settings | ||
Automatic output time | ||
Data collection function | File collection settings | |
Collection source | EcoWebServerⅢ | |
Edgecross | ||
Automatic collection settings | ||
Automatic collection timing | ||
Collection period | ||
Retention period | ||
Data input function | Data input | |
Export | ||
Import | ||
Calculation function | Available measuring point | |
Automatic calculation | ||
Available measuring point | ||
Data output function | Data output | |
Auto output settings for data file | ||
Output measuring point | ||
Maintenance function | Backup | |
Restore | ||
Diagnosis settings | Equipment setting | |
Energy-loss factor setting | ||
Calculation measuring point for diagnosis setting | ||
Available measuring point | ||
Electricity rate setting | ||
Diagnosis function | Energy-loss diagnosis | |
Energy-loss extraction | ||
Energy-loss factor diagnosis | ||
Improvement result check | ||
Automatic diagnosis | ||
Diagnosis panel | ||
PC’s Operation Environment | OS | |
Language version | ||
CPU | ||
Memory | ||
Hard disk | ||
LAN | ||
USB connector (Type A) | ||
CD drive | ||
Spreadsheet *2 | ||
Display resolution | ||
Input device |
Energy Saving Supporting Devices |
Application Software |
Energy Saving Support Software EcoAdviser |
Energy saving data analysis and diagnosis software |
Register a collection source and its measuring points. |
EcoWebServerⅢ, Edgecross |
Max. 20 units |
Max. 5680 points Max. 255 points per unit Demand period (15 minutes): Max. 284 points per unit Demand period (30 minutes): Max. 282 points per unit Demand period (60 minutes): Max. 280 points per unit Max. 256 points per unit Data type: BOOL, INT, UINT, DINT, UDINT, REAL, LREAL |
Register a measuring point other than collection sources. |
Register a measuring points to extract data of one product from multiple types of products. |
Select from collection sources’ measuring points or manual input measuring points. |
Register a measuring point to calculate measuring points with each other. |
Select from collection sources’ measuring points, manual input measuring points, or product type time period measuring points. ∙ Max. 200 points can be registered per calculation formula. ∙ Max. 4000 letters can be used per calculation formula. |
Register a measuring point to calculate specific consumption. |
Select from collection sources’ measuring points, manual input measuring points, product type time period measuring points, or calculation measuring points. |
Select from time series chart, box plot, pie chart, scatter plot, histogram, or pareto chart. |
Select from hourly, daily, monthly, or yearly. * For an analysis method of box plot, this is set to hourly. |
Create a dashboard with graph and measuring point data panels arranged. |
Graph panel (created with graph function) Diagnosis panel (graph/table of diagnosis result) Numeric panel (collected measuring point data) Image panel (image file) |
Display the created dashboard on EcoAdviser. |
Set the automatic update of graphs and measuring point data. |
Set the display of the tab for sheet switching. |
Set the automatic switching of the sheet at regular intervals. |
Output the created dashboard to the HTML file. |
Set up the report format. |
Max. 24 report settings (In one setting, output items of daily, monthly, and annual report are saved.) |
Daily report : Max. 320 items, 16 items per sheet × 20 sheets Monthly report : Max. 320 items, 16 items per sheet × 20 sheets Annual report : Max. 320 items, 16 items per sheet × 20 sheets |
Select from collection sources’ measuring points, manual input measuring points, product type time period measuring points, calculation measuring points, or specific consumption measuring points. |
Create the daily report of a specified day and save it in the Excel format. |
Create the monthly report of a specified month and save it in the Excel format. |
Create the annual report of a specified year and save it in the Excel format. |
Set the automatic output of reports. |
Set the time of automatic output of reports. |
Collect the logging files stored in the collection sources. |
Zoom (1 min.) data file, Demand (daily) data file |
Historical data file |
Set the data collection for each file type. |
EcoWebServerⅢ : Collection time specified by the user Edgecross : Collection period specified by the user |
Set the collection period on daily/monthly/annual basis. |
Set the retention period for each file type. 15/30/60-minute basis data: 2 to 10 years (Default: 10 years) Daily basis data: 2 to 10 years (Default: 10 years) Monthly basis data: 2 to 10 years (Default: 10 years) Annual basis data: 2 to 10 years (Default: 10 years) Diagnosis data: 2 to 10 years (Default: 10 years) Diagnosis source data: 62 days |
Input 15/30/60-minute basis data of each measuring point for a user-specified period. Max. 256 measuring points can be selected simultaneously. Specified period: Max. 31 days |
Output 15-min/30-min/60-min/24-hour basis data of each measuring point for a user-specified period to the Excel file. |
Input 15-min/30-min/60-min/24-hour basis data of each measuring point based on the imported Excel file. |
Select from product type time period measuring points, calculation measuring points, or specific consumption measuring points. * Max. 256 measuring points can be selected at one time. |
Automatically calculate measuring point data. |
Select from product type time period measuring points, calculation measuring poins, or specific consumption measuring points. |
Output the collected measuring point data, which is saved in the file. |
Set the automatic output of data files. |
Select from measuring points, manual input measuring points, product type time period measuring points, calculation measuring points, or specific consumption measuring points. |
Back up the setting values and data to the folder |
Restore the setting values and data backed up from the specified folder |
Register the equipment information for energy-loss diagnosis |
Set the energy-loss factor for equipment |
Set the calculation measuring point for energy-loss diagnosis. |
Select from measuring points. *Demand measuring points are excluded. |
Set the currency unit and electricity rate per 1 kWh to convert energy consumption into the amount for diagnosis. |
Diagnose the following two items for equipment. |
Extract energy-loss on the five focusing points for energy saving or the standby power for each equipment to rank in order of energy-loss. |
Diagnose energy-loss factors for any points for energy saving of any equipment. |
Compare the data of two periods to check the effect of energy saving improvement activities. |
Execute automatic diagnosis of energy-loss and its factor. |
Save the graph ot table of energy-loss extraction or energy-loss factor diagnosis result. |
Microsoft Windows 10 Pro/Enterprise/IoT Enterprise (64-bit) Microsoft Windows 11 Pro/Enterprise (64bit) |
Japanese, English, Simplified Chinese |
Intel CoreTM i3-550 (recommended) |
4GB or more |
Software: 4GB or more Data: 20GB or more *1 |
10/100/1000BASE-T×1 |
1 connector (for connecting the hardware key) |
1 drive (for installing EcoAdviser) |
Microsoft Excel 2016 (32-bit/64-bit) Microsoft Excel 2019 (32-bit/64-bit) Microsoft Excel 2021 (64bit) |
1024×768 pixels or more |
A mouse and keyboard |
*1: If you set the storage period of each data and the registration number of each measuring point to the maximum, this capacity will be necessary.
*2: You cannot use the Excel that has been purchased from Microsoft Store. Use the desktop version of Excel.