Tags are data sets for GENESIS64™ to access external devices. The number of data sets used in runtime of GENESIS64™ are counted. In the example below, a device value of a programmable controller = 25 and an SQL statement that refers to the last week temperature data are targets counted.
Difference of counted tag
Type of data | Real-time data | Historical data |
---|---|---|
When using Hyper Historian™ | GENESIS64™ tag | Hyper Historian™ tag |
When using Hyper Historian™ Express | GENESIS64™ tag | GENESIS64™ tag |