Factory Automation

Update : 2022/11/15

TOSEI (THAILAND) CO., LTD.

Device Partner

Tosei (Thailand) Co., Ltd. is a professional in In-Line Measuring system under ACCRETECH brand. we specialize in development and manufacture of automated measuring instruments for production line of cars, bearing, home electric appliance, various electronic products and etc.

Address

Amata City Chonburi Industrial Estate, Phase 6C, 700/633 Moo 7, Tambol Donhuaroh, Amphur Muang, Chonburi Province 20000

Measuring system for metal machining process (Grinding / Turning / Machining)

Machine control gauge using in Grinding machine to control grindstone depth of cut speed and Real time workpiece’s size control. Grinding wheel balancer is useful to reduce more than half of normal Grinding wheel exchange time. Grinding monitoring system is useful in the following applications by measuring the acoustic emission signals which is generated by the contact between the grinding wheel (the cutting tool) and workpiece or the dresser, 4 main propose are Gap control, Dressing control, Crash detection and Failure analysis.

Air / Electric Micrometer for Post process measurement

Various measuring applications (Dimension, GD&T, Etc.) can be measured by our Air / Electric Micrometer. High precision and can be customize to meet with customer requirement.