Factory Automation

Update : 2023/07/05

SIAM SMART SOLUTIONS CO., LTD.

System Integration Partner

JIG, Equipment, Machine, Automation Line Automation system, IoT system
Digital Transformation(DX), SMART Factory, SMART Farm, Traceability system

Address

129 Chaloem Phrakiat Ratchakan Thi 9 Rd., Kwang Dokmai, Khet Prawet, Bangkok 10250

Compression strength test machine

The compression testing machine is an automatic machine that employs a PLC Mitsubishi to control the electric cylinder from SMC via CC-Link system. When the machine performs the compression testing, it will record the data according to the specified details onto a memory card for convenient use in the future.

Weighing scale for chemical substances.

The chemical weighing machine is an automatic device that utilizes PLC Mitsubishi to control the weighing of chemicals, in order to separate the weight of each type of substance according to the desired requirements and to collect data of the weight of each type of substance.

Cobot

Controlling Cobot with PLC Mitsubishi for interworking with automated machinery systems, the working process of the machinery involves using Cobot to pick up materials from trays and place them on the machinery, replacing human labor.