Controllers MELSEC iQ-R Series Product features -Concept-

Concept
As the core for next-generation automation environment,
realizing an automation controller with added value while reducing
TCO
*1
To succeed in highly competitive markets, it's important to build automation systems that ensure high productivity and consistent product quality. The MELSEC iQ-R Series has been developed from the ground up based on common problems faced by customers and rationalizing them into seven key areas: Productivity, Engineering, Maintenance, Quality, Connectivity, Security and Compatibility. Mitsubishi Electric is taking a three-point approach to solving these problems: Reducing TCO *1 , increasing Reliability and Reusability of existing assets.
As a bridge to the next generation in automation, the MELSEC iQ-R Series is a driving force behind revolutionary progress in the future of manufacturing.
- *1. TCO: Total Cost of Ownership