Factory Automation

Solutions Carbon neutral

Aiming for a decarbonized society

As a leading manufacturer, Mitsubishi Electric considers contributing to carbon neutrality our major mission.
In addition to FA equipment and power distribution control equipment,
we support our customers' sustainable business activities by utilizing IoT platforms as well as applications for visualization, analysis, and diagnosis.

Buildings

Case06 To eliminate temperature unevenness and achieve energy saving at the same time

  • Improvement
Issues
The building is large that the air conditioning isn't evenly distributed (Some areas are hot while some are cold).
We want to save more energy, but we can't sacrifice comfort.
Solution
  • An air conditioner and Air Conducting Fan are used in combination to firmly circulate cold and warm air even in large spaces
  • Achieving energy saving while maintaining comfort by increasing heating and cooling efficiency

Circulation effect improves indoor temperature distribution

Circulation effect improves indoor temperature distribution

Even if the setting temperature of the air conditioner is changed, it is possible to save energy and electricity effortlessly while maintaining comfort

Even if the setting temperature of the air conditioner is changed, it is possible to save energy and electricity effortlessly while maintaining comfort
Benefits
  • Even in large spaces, air conditioning is distributed to every corner and the temperature environment is improved
  • Reduce electricity bills with more conservative air conditioning temperatures while maintaining comfort

Cases