Start main contents

News

News Release Archives

Note that the releases are accurate at the time of publication but may be subject to change without notice.

FOR IMMEDIATE RELEASE No.2883

Mitsubishi Electric to Unveil World's Largest High Definition Video Display

Diamond Vision® by Mitsubishi Electric to unveil a record-breaking 77.69' x 329.65' display, using revolutionary Real BlackTM LED technology

TOKYO, November 18, 2014- Mitsubishi Electric Corporation (TOKYO: 6503) announced today that it will unveil a Diamond Vision display at 1535 Broadway in New York City's iconic Times Square that exceeds 4k ultra-high-definition pixel density. The screen is a massive 25,610-square feet, and with a pixel density of 2,368 x 10,048, it will be the highest resolution LED video display in the world. The installation will employ a Mitsubishi Electric Diamond Vision AVL-ODT10 large-scale display, which provides true 10mm pixel pitch spacing and uses a 3-in-1 surface mount LED (SMD) featuring Mitsubishi Electric's revolutionary Real Black LED technology.

"With 23,793,664 individual physical pixels, a video quality display of this size and density is a milestone in the industry. It exceeds 4k resolution by nearly 15 million pixels," says Todd Stih, national sales manager, Mitsubishi Electric Power Products, Inc.

Due to the very high resolution and pixel density of the display, Mitsubishi Electric supplied a special control system to provide pixel-to-pixel mapping of content and life-like images. The image area of the screen can be segmented to display multiple pixel-for-pixel 1080 HD or 4k images simultaneously. The display canvas allows for two 4k images to be displayed side by side, with pixels remaining in the height and width for other content.

The use of the Real Black LED technology allows for deep, rich black levels and unsurpassed vertical viewing angles in an outdoor LED display product. The characteristics of Real Black LED technology will ensure that Times Square crowds have a clear view of the screen up close and in bright sunlight conditions.

"We have worked on a number of record-breaking projects, but working with this type of pixel density and installing it in a 24/7 live environment presented unique challenges. However, we delivered the display modules earlier than scheduled due in part to great cooperation and teamwork with the project team at Vornado Realty Trust, our customer," says Mike Brosko, operations manager, Mitsubishi Electric Power Products, Inc.

Mitsubishi Electric has significant experience with traditional lamp-based RGB LED display products as well as 3-in-1 SMD technology. Based on this experience, the Real Black LED technology was developed and introduced to overcome the shortfalls of these traditional technologies and marks what Mitsubishi Electric believes is the most significant advancement in large-scale outdoor LED technology since the conversion from CRT to LED in the 90's. The technology features black LEDs that provide a continuous black face to the display not previously possible with red, green and blue (RGB) lamp LED products or traditional SMD products which utilize white-faced LEDs. "The Real Black LED technology revolution is just beginning with fifteen other displays using Real Black LED technology coming on line in North America over the next few months," says Stih.

Rendition of Diamond Vision screen at Marriott Marquis Hotel

Rendition of Diamond Vision screen at Marriott Marquis Hotel

Diamond Vision is a registered trademark of Mitsubishi Electric Corporation.
Real Black is a trademark of Mitsubishi Electric Power Products, Inc.

Inquiry