News Release Archives
Note that the releases are accurate at the time of publication but may be subject to change without notice.
FOR IMMEDIATE RELEASE No.2892
Mitsubishi Electric to Launch 7.0-inch WVGA TFT-LCD Module
Achieves market-leading vibration resistance and operating temperature range
TOKYO, December 17, 2014- Mitsubishi Electric Corporation (TOKYO: 6503) announced today the coming launch of a new 7.0-inch WVGA TFT-LCD module for industrial applications such as construction, agricultural vehicles, factory-automation and weaving equipment. The module's 6.8G vibration-resistant acceleration is seven times greater than that of conventional modules, which it combines with -40 to 85 degrees Celsius operating temperature range, 1,500cd/m2 super-high brightness and high contrast ratios. Sample sales will begin February 27 through Mitsubishi Electric offices worldwide.


Mitsubishi Electric will strengthen its wide lineup of industrial modules with the new TFT-LCD module, which meets increasing market demands for resistance to extreme vibration and temperatures for versatile application and installation.

Product Features
| 1) | High vibration resistance for construction and agricultural applications
|
||
| 2) | Durability for extreme outdoor environments
|
||
| 3) | High brightness and contrast ratio
|
||
Sale Schedule
| Product | Model | Shipment | Production |
| 7.0-inch WVGA TFT-LCD Module |
AT070MJ01 | February 27, 2015 | 2,000 units per month |
Inquiry
Customer Inquiries
Mitsubishi Electric Corporation