News Release Archives
Note that the releases are accurate at the time of publication but may be subject to change without notice.
FOR IMMEDIATE RELEASE No. 2978
Mitsubishi Electric to Expand Lineup of 3.5 GHz-band GaN-HEMTs for 4G Mobile-communication Base Transceiver Stations
New products support macro and small cell BTS
TOKYO, December 22, 2015- Mitsubishi Electric Corporation announced today that it would expand its lineup of Gallium Nitride High Electron Mobility Transistors (GaN-HEMTs) for use in Base Transceiver Stations (BTS) operating in the 3.5GHz band of fourth generation (4G) mobile communication systems. The four new GaN-HEMTs offer output power and efficiency levels that are among the highest currently available according to company research as of December 22. Samples will be released starting February 1.

| (From left) MGFS53G38ET1, MGFS50G38ET1, MGFS38G38L2 and MGFS37G38L2 GaN-HEMTs for 3.5-GHz 4G mobile communication BTS use |
As a result of the deployment of Long Term Evolution (LTE) and LTE-Advanced mobile networks, needs are
rising for BTS that can offer increased data volume, smaller size and lower power consumption. In response, Mitsubishi Electric has developed the new GaN-HEMTs designed for use in macro BTS and large numbers of micro cells that mobile network operators are employing to increase the data capacity of their advanced 4G networks built with LTE and LTE-Advanced technologies.

Going forward, Mitsubishi Electric will continue to expand its GaN-HEMT lineup for use in different output power and frequencies, and in mobile communication systems beyond 4G.

Going forward, Mitsubishi Electric will continue to expand its GaN-HEMT lineup for use in different output power and frequencies, and in mobile communication systems beyond 4G.
Product Features
| 1) | Expanded product line-up
|
||||||||
| 2) | GaN-HEMT and transistor optimization for high efficiency
|
||||||||
| 3) | Size reduction
|
||||||||
Inquiry
Customer Inquiries
Mitsubishi Electric Corporation