Factory Automation

Service & Support

e-learning courses (Vietnamese)


A collection of frequently used FA terms and example sentences! FA field glossary

The online edition requires a screen resolution of XGA (1024 x 768) or higher.
The offline edition can be downloaded by clicking on the following icon.
For further information about methods of expanding data in the EXE edition, refer to "Using the EXE edition data" located at the bottom of the page.

Vietnamese

Courses Online edition (compatible with tables) Offline edition
EXE edition PDF edition
FA Equipment for Beginners PLCs -
HMIs
Inverters
Servos
Industrial Network
Positioning
Process Control System
Industrial Robots
Power Distribution Control Products
Machinery Safety
Basic edition / Advanced editions Programmable Controllers MELSEC-iQ-R/Q/L/FX MELSEC iQ-R Series Basics -
MELSEC iQ-F Series Basics - -
MELSEC-Q Series Basics -
MELSEC-L Series Basics - -
GX Works2 Basics -
GX Works2 Advanced -
GX Works3 (Ladder) -
PLC Programing Basic (Ladder) -
PLC Programing Basic (ST) -
Applications of Programming - -
Applications of Programming (MELSEC iQ-R Series)
Efficient Programming -
CC-Link IE TSN -
CC-Link IE Controller Network - -
CC-Link IE Controller Network (MELSEC iQ-R Series) -
CC-Link IE Field Network - -
CC-Link IE Field Network (MELSEC iQ-R Series) -
CC-Link - -
CC-Link (MELSEC iQ-R Series) -
Ethernet - -
Ethernet (MELSEC iQ-R Series) -
Intelligent Function Module - -
Intelligent Function Module (MELSEC iQ-R Series) -
Serial Communication - -
Serial Communication (MELSEC iQ-R Series) -
Positioning - -
Positioning Control (MELSEC iQ-R Series) -
MELSEC Process Control System Basics -
PLC System Maintenance -
Safety CPU Basics (MELSEC iQ-R Series) -
Safety Controller Basics -
Manufacturing Visualization Basics (MELSEC iQ-R series MES interface module) -
Human-Machine Interfaces(HMIs)-GOT GOT Basics (GT16, GT Designer3) - -
Inverters-FREQROL FREQROL Basics 800 (Operation) - -
FREQROL Basics 800 (Function) - -
FREQROL Basics 800 (Maintenance) - -
FREQROL Basics (Operation) - -
FREQROL Basics (Function) - -
Inverter energy saving course -
AC Servos-MELSERVO MELSERVO Basics (MR-J4) -
MELSERVO Basics (MR-J4-GF Servo Amplifier I/O Mode) -
MELSERVO Basics (MR-JE Modbus) -
SIMPLE MOTION Module - -
SIMPLE MOTION Module (iQ-R CC-Link IE Field) -
SIMPLE MOTION Module (iQ-F) -
MOTION Module Basics (iQ-R·RD78G(H)·Startup) -
MOTION Module Basics (iQ-R・RD78G(H)/Position Control) -
MOTION Module Application (iQ-R・RD78G(H)・Interpolation/Synchronous Control) NEW -
MOTION CONTROLLER Basics (Hardware) - -
MOTION CONTROLLER Basics (Real Mode:SFC) - -
MOTION CONTROLLER Basics (iQ-R·RnMTCPU)
MOTION CONTROLLER Application (Virtual Mode) - -
Linear Servo -
Industrial Robots-MELFA MELFA Basic and Maintenance (FD Series) - -
MELFA Basic and Maintenance (FQ Series) - -
MELFA Basic and Maintenance (FR Series D Type)
MELFA Basic and Maintenance (FR Series R Type/Q Type)
Power Distribution Control Products Low-Voltage Circuit Breaker -
Contactors and Motor Starters -

Using the EXE edition data

[How to expand the downloaded file]

Download the file to a folder of your choice.
When you decompress the downloaded file, a folder will be created.

Decompression method 1) When using an OS that features a ZIP-compatible decompression tool

Right click on the downloaded file.
Select "Expand All".
Specify the expansion destination, and click on the "Expand" button to decompress the file.
If "Expand All" is not displayed, use decompression method 2) below.

Decompression method 2) When using an OS which does not feature a ZIP-compatible decompression tool

If your OS does not feature a ZIP-compatible decompression tool, please obtain a decompression tool separately.
Use the decompression tool to decompress the file.
Decompress the file to a directory.

* The user accepts full responsibility for the use of a decompression tool.

[How to start]

Double click on "exe file" in the folder that has been created.

Inquiries