Solutions Total Maintenance

In today’s dramatically changing business environment, the impact of sudden equipment downtime on corporate profits is enormous, and an increasing number of businesses are implementing planned equipment maintenance with the aim of achieving non-stop factories.
Meanwhile, the manufacturing industry faces another major issue of passing down the expertise of highly experienced employees.
Case12 Restoring FA device programs on-site immediately
Corrective
Maintenance
Equipment level
In the event of PLC failure or a dead battery, new equipment and a computer for writing programs must be prepared, which means recovery takes a long time.

Enable easy backup/restoration of FA device programs and parameters
The GOT Backup/Restoration function allows users to back up programs and parameters of FA devices such as PLCs to a GOT SD memory card or USB memory. Programs and parameters can be easily restored from GOT to FA devices when the devices need to be replaced.


By performing backups in advance, it is possible to restore FA devices from GOT on-site without a PC in the event of an FA device failure, which reduces downtime.