News
Mitsubishi Electric Develops Edge-device Language Model for Domain-specific Manufacturing
Language model for manufacturing industry operating on edge devices
TOKYO, June 18, 2025 - Mitsubishi Electric Corporation (TOKYO: 6503) announced today that it has developed a language model tailored for manufacturing processes operating on edge devices. The Maisart®1-branded AI technology has been pre-trained with data from Mitsubishi Electric’s internal operations, enabling it to support a wide range of applications in specific manufacturing domains. In addition, the model leverages a uniquely developed data-augmentation technique to generate responses optimized for user-specific applications.
The widespread adoption of generative AI is accelerating the use of large language models (LLMs). However, the significant computational and energy costs associated with LLMs are a growing concern. Additionally, there is increasing demand for generative AI solutions that can operate in on-premises2 environments due to data privacy and confidential information management requirements.
In response, Mitsubishi Electric has developed a domain-specific language model by training a publicly available Japanese base model with the company’s proprietary data from its own business domains, including factory automation (FA). Using training data generated through the company’s original augmentation techniques enabled effective, task-specific fine-tuning. The resulting model is compact enough to run on limited hardware resources, making it suitable for environments with constrained computing capabilities such as edge devices, as well as for on-premises operations such as call centers that handle sensitive customer information.
The language model was developed as part of the AWS Japan Generative AI Accelerator Program3 provided by Amazon Web Services Japan G.K. AWS Japan provided support for the development, including computing resources such as GPUs4 and AWS Trainium5 for language-model training, assistance in building distributed training environments, AWS credits, and scientific support from the AWS Generative AI Innovation Center.6
- 1
"Mitsubishi Electric’s AI creates the State-of-the-ART in technology" :
Mitsubishi Electric’s AI technology brand aimed at making every device smarter.
- 2
A model in which a company or organization builds, manages, and operates its IT infrastructure (servers, network equipment, etc.) within its own facilities, as opposed to cloud-based models that operate over the internet.
- 3
This is a Japan-specific support program that was developed by AWS in 2023, building on a large-scale language model (LLM) focused development support program, and launched in July 2024.
- 4
Graphics processing unit for image processing and parallel computation at high speed to significantly reduce LLM training time.
- 5
AWS-developed custom chip specifically for cost-efficient, high-performance training of AI models.
- 6
Inquiry
-
Customer Inquiries
Information Technology R&D Center
Mitsubishi Electric Corporation