External Environmental Evaluation
ISO Certification
Mitsubishi Electric has obtained company-wide multi-site ISO 14001:2015 certification in order to strengthen compliance by the Company as a whole and to further strengthen its contribution to the environment by ensuring that business operations are based on environmental plans.
As of this report, approximately 90% of associated companies with manufacturing sites covered herein have obtained ISO 14001:2015 certification, while the certification rate across all associated companies stands at around 50%.
Third-Party Assurance
To ensure the reliability of its disclosures, Mitsubishi Electric obtains third-party assurance from an external assurance provider for its greenhouse gas emissions, water intake and wastewater volumes.
For other initiatives and external evaluations, click below: